This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI TI expert,
I have the requirements as below:
Vin=2.5~3.3V
Vout=12V
Iout max=80mA
TPS61096A is selected for our design to meet the above requirements.
But when I try to generate the schematic with the WEBENCH Power Designe, an error happen to warn the current limit is exceeded, but the max current is 0.5A.
It look the tool set the current to 0.05A. Please check it. and also please to check if TPS61096A can meet my requirement?
Thanks
Hi Allen,
the input current is only 0.5A peak for TPS61096A, not output current.
please try TLV61046A for your application.