This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55288: Not working -

Part Number: TPS55288


Hi Zack,

I have finally received the boards back from the manufacture. They are not working properly I only get an output of 1V. The manufacture has done x-ray to confirm that the device is properly soldered to the board.

It does not matter if I use 20V or 3.3V, I always get 1V output.

I have not been able to check the register since I need at least 3V for the communication to work.

Any advice on what to do next?

Regards,

Marlon