This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC3854: Device with PSPICE model similar to UC3854?

Part Number: UC3854
Other Parts Discussed in Thread: UCC28180

Hi,

For a new design my customer is considering PFC UC3854 as it can also be used as a Buck (and not only as a boost) with 80-265Vac and 130Vdc as output, 15A continuous and 25A pk. However this device does not have any simulation model available (pspice, Tina...). Could you please recommend me a device with above specs and with simulation model so to enable customer simulate the behavior?

Thank you,

Antonio