Other Parts Discussed in Thread: TPS27SA08
I want to use the 3 x TPS22810 load switch in parallel for a 12V / 7A power rail,and I have below questions:
1. As the Rds(on) for each load switch might differs, how can we ensure the equal balance of load current sharing. One of the load switches will tends to have more current flowing than the others. This will result having that particular load switch to be burnt out easily as compare to the others.
2. The turning-off the load switches, the turn off delay for each of the load switch will be of different timing. so one might be turning off faster than the others. And this result the slower turning off load switch needs to take the share of the load current. This adversely will cause the slower one to be overloaded and burnt out.