Hi team,
Customer used to design MODE pin with 121kOhm, but they are going to implement it with 90.9kOhm for the current board. As per the related thread, the tolerance of MODE pin is 5%. Then, I believe API and BB triggering level might be on unknown status if they use 90.9kOhm for MODE resistor. Does it have any expected problem with the output operation?