Part Number: TPS2663
Other Parts Discussed in Thread: TPS2640, , TPS1663
Dear TI Team
When operating with an input of 24V and no load, the phenomenon that the FLT pin is asserted occurs as shown in the following post.
Probably the Reverse current protection is working as shown in the following post.
https://e2e.ti.com/support/power-management/f/power-management-forum/865182/tps2662-flt-indication-if-output-current-is-very-small
After starting with no load, the load was reduced by about 240mA, but the FLT terminal was still asserted.
(There is no problem even if the OUT terminal has no load. 24V is output)
I would like you to answer the following questions.
1. Is there a problem such as not being able to use other functions if the TPS2640 is operated with the FLT pin asserted?
(I think it's a problem not to be aware of other protections)
2. Is there a way to prevent the FLT pin from asserting under no load?
(I think that Vout is probably higher than Vin when there is no load, but please let me know if there is any countermeasure.)
Best Regards,
Y.Ottey