Part Number: UCC29002
Other Parts Discussed in Thread: UCC28951, PMP8740
Hello,
In an earlier thread, I had questions about UCC29002/1 in no-Rsense and low-side configuration. I reference the thread here as the schematic and info are related.
I built the system with three 600W PSFB Modules that have independent input source. The output of the three modules is combined to a 1800W/-48V DC bus. Each module uses UCC29002/1 load sharing controller.
Observations:
- Saturation Issue Case 1:
- ALL three modules are powered up.
- Activate only one of two of the PSFB converter.
- Result: UCC29002/1 ADJ pin will saturate (7mA goes through Q2) on ONLY one of the UCC29002/1 controllers under no LOAD.
- Saturation Issue Case 2:
- ALL three modules are powered up.
- Activate the PSFB converter modules before closing the output switch Q1.
- Result: UCC29002/1 ADJ pin will saturate (7mA goes through Q2) on ONLY one of the UCC29002/1 controllers under no LOAD.
- Load Sharing Bus (LS) Issue:
- Two out of three modules are powered up
- Result: LS BUS seems to be held low unless the disconnect it from the non-powered-up module.
- Regulation issue:
- All three modules are active.
- 1500W Load.
- The load is shared among all three modules with 3% error.
- Sometimes, after running the system for several minutes, one of the LS controllers will share half the current the other two modules do.
- Load-step:
- All three modules are active.
- The maximum load can star-up with is 1200W, which is the maximum capacity of two modules out of three.
Questions:
- Please advise what could cause observation 1 given that it happens 50% of the time and RADJ is carefully selected and has enough margined for regulation.
- Please advise what could cause observation 2 and whether I should connect Radj after the output switch Q1.
- Please advise regarding Observation 3. Is there any issue if:
- Only one or two of the three modules are powered-up > The LS pin on non-powered controller will see a maximum of 8V since the bus is shared. That goes into the absolute maximum rating of LS-PIN when the chip is not powered. If that is an issue, any suggestions?
- All modules are powered up but only one or two of the three modules PSFB Converter are active? Do I need to disable the LS controller if the module is powered up but the PSFB converter is not enabled? Suggestion?
- Observation 4: What could cause one of the LS controllers to lose regulation?
- Observation 5 could be due enabling LS at the startup circuit on UCC29002-1. I am planning to test with UCC29002 but I am not sure about one statement in the datasheet: “Both the load share driver and the adjust amplifiers revert to normal operation as soon as the measured current exceeds 80% of the average per module current level represented by the LS bus voltage”. Does that mean output current has to reach 80% of the maximum load current for the controller to revert to normal? What if the load is dynamic (i.e., 25% only)?
Thanks