Other Parts Discussed in Thread: TPS2121, , TPS2115, TPS2116, TPS2113A, TPS2120
Hi,
Our project decided to use TPS2121 for Power MUXing two 5V sources for redundancy. However, due to the situations all around the world, TPS2121 has been out of stock and production of our PCB boards have been suspended. We checked on the schedule for restocking but the dates are off our target schedules. Therefore, we decided to instead use TPS2115ADRB.
We decided to let an external 5V be connected to IN2 and a 5VUSB to IN1. We designed it such that, by default, the 5V supply comes from the external 5V supply and switches to 5VUSB in case the external 5V drops. Then I decided to use the STAT pin to drive an LED to turn on when the Output 5V is supplied by the 5VUSB instead of the default 5V external.
I am attaching here the screenshot of the sample schematic for using the TPS2115A.
I just would like to confirm if this design will work according to what we have in mind. BTW, I am operating the TPS2115 in autoselect mode. +5VDC comes from a 5V regulator IC, VUSB is the 5VUSB, and +5V is the output of the TPS2115ADRB.
Any suggestions are also welcome. Thanks.