Hi TI Team,
Lately I've designed a board referring to the Eva board and right now I'm testing out the cell balancing features.
The data obtained using the cell voltage monitor after enable cell balancing and my configuration for cell balancing is as below.


My questions are
- The cell balancing features seems like working well but why is the cell not able to balance up in the end. Is there any problem with my configuration setting?
- I even tried to set 120minutes balance time for cell2,3,4,5 and 0 minutes balance time for cell1,6 but the voltage of each cell still didn't balance up.
I'm charging my 18650 cells using DC power supply with output setting 25.2V and 2A.