Other Parts Discussed in Thread: TPS560200-Q1
Dear Sir/Madam
Our PCB requires 5V and 3.3V. Max Vin can be 24V
The 3.3V will be used for all the wifi and uC circuits, max 350mA
The 5V is needed as a pullup on a PWM signal to a fan, max few mA.
I intended to use this device to generate the 5V, then use a simple SOT23 LDO to generate 3.3V. Would this be the best way or can you offer any better suggestions?
Can we also use following inductor with this device?
Murata | LQH43PN100M26L |