This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: Are all BQ76952 devices functionally same? Will devices support i2c?

Part Number: BQ76952

Hi,

I have finished work for bq76952 with communication interface i2c, No CRC enabled. Since they are out of stock now. I would like to use other devices in the devices comparison table

BQ76952 I 2C N Disabled

BQ7695201 SPI Y Disabled

BQ7695202 I 2C Y Enabled, set to 3.3 V

BQ7695203 SPI Y Enabled, set to 5 V

BQ7695204 SPI Y Enabled, set to 3.3 V

My question is, by changing the settings-configuration-comm type settings.. are all devices functionally the same, In other words by changing register settings can I convert bq7695202 to bq76952, bq7695204 to bq76952?