Other Parts Discussed in Thread: UCC28070
Hello,
we are testing a 3850W PFC module, with UCC28070. During the tests we have seen that at full load if the input voltage goes down from 230V to 225V there is an input current raise with an increase of the output voltage that some time it makes happen an overvoltage protection. I think it is related to the level change of the UCC28070 linear multiplier.
We have increase the output capacitors to 4x470uF, without solve the problem.
The output voltage is 390Vd so the Vsense and Vinac resistor are:
Rtop=3200k Rbottom=24.9k
The Rimo=47k
The voltage error compensation is:
Cpv=100nF+47nF RZV=82k CZV=1.5uF
I enclose 2 pictures, the first with no problem the second with the problem.
Traces 1=input current 2=switch current 3=output voltage 4=VAO
No problem without stop input current
Problem with the stop input current