Part Number: LP8545
Other Parts Discussed in Thread: LP8556, TPS61177, TPS61187
Hi guys,
My customer wants to use the LP8545 but they have a question. They need to enable the Iset pin to set the current threshold, but according to the datasheet the Iset pin is inactive until enabled via EEPROM. However, there is a note about the EEPROM:
"EEPROM NVM can be programmed or read by customer for bench validation. Programming for production devices should be done in TI production test, where appropriate checks will be performed to confirm EEPROM validity. Writing to EEPROM Control register of production devices is not recommended. If special EEPROM configuration is required, please contact the TI Sales Office for availability."
So, can they use a host MCU to adjust settings in EEPROM after the parts boot up? or are they supposed to tell you guys what settings they want and are stuck with them after production test?
This note is confusing, so some elaboration would be nice on what that means exactly. Is it just that "EEPROM Control Register" with address 72h that is off limits, and the rest of the device settings are fine to change at will?
Thanks,
Brian