Part Number: TPS61196
Hello
when TPS61196-Q1 work in master/slave mode,the OVP was determined by Slave or Master chip ? and why Slave's OVP voltage must be 3% higher than the voltage at the Master's OVP pin ? thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sean
" The slave's OVP pin voltage must be 3% higher than the voltage at the master's OVP pin. " Acording to this demand, Slave's setted OVP of Vboost will less than Master's setted OVP of Vboost, so if OVP happened, it should trigger Slave's OVP first, then trigger Master's OVP latter. is it right ?