Part Number: BQ78350-R1
Other Parts Discussed in Thread: BQ76930, BQ78350, , STRIKE
Hi all,
First of all, I'm very thankful that you have such good support.
We have a battery pack (bq76930+bq78350+10s6p) that has been tested for ESD.
The battery pack did not pass because a short power glitch on PACK +/- switch off the complete system somehow.
After a few ESD shots, the battery was always completely off, as in shutdown. After that I thought that the battery was doing "Voltage Based Shutdown" the "Shutdown Voltage" value was set to 0.The battery was passed with this settings.
I suspect that a partial reset can occur because the lifetime data will not be updated with new data. (Not as in normal shutdown.)
The battery starts normally with "Voltage at TS1 pin> VBOOT".
Our system is designed as here described "Avoiding ESD and EMI Problems in bq20zxx Battery Pack Electronics "
The question is if that happens what I think and why "Shutdown Voltage = 0" can help. Shutdown Time = 10sec.
Thank you for your answer.
Best regards
Adam