Part Number: BQ25601
Other Parts Discussed in Thread: BQ24266,
We want the device (VSYS) to be powered-up whenever VBUS is available, regardless of the battery condition. With the battery physically disconnected, we notice that VSYS oscillates between 4.2V and 3.8V, so the device does not power-up. See the attached picture. How can we disable this VSYS oscillation under the SW control, so that the device (VSYS) can be powered on, and remain powered on whenever VBUS is available, even when the battery is completely depleted or removed?