Part Number: BQ24610
Hi,
When the CE is enable, refering to waveforms on Page 12(BQ24610 datasheet), I see that VCC、VREF、REGN signals are normal. But PH and LODRV are abnormal. After the chip enters the charging mode, it lasts about 200ms and then it quits the charging mode. Because of CE enable, it happens every 2 seconds cyclically. The STAT1 LED blinks. Whether some conditions are triggered, it makes bq24610 to enter the charging mode and quit immediately. I read Section 9.3.7,but I didn't know how to solve it.
What is the reason? What should I do?
Thanks!
Regards!