Other Parts Discussed in Thread: TPS61088
Hello TI,
1. Testing on own design PCB which is design as per the TI reference Design & Guidelines
2. Use 5V/ 2A adapter with BQ24773 for testing
3. design for 1 cell(2200mA) charging
There is some question about the BQ24773 working,
1. BQ24773 can work without battery with load on default setting(Without configuration) for initial system ON..?
2. BQ24773 can work with load on Default setting if yes, what is the minimum load handle the system ..?
we are design the system for specific application, please clear the below mention points
1. BQ24773 can work standalone..?
2. BQ24773 can work with or without battery ..?
3. BQ24773 can able to work like UPS system ..?
please refer the thread for more details of design 
Thanks and Regards,
Rahul Surawase