Part Number: BQ40Z80
Other Parts Discussed in Thread: BQSTUDIO
Hello!
In the BQ40z80 Tech.Ref i can see information about Pin 13 likе this :
>>Set Settings:Pin Configuration[MFP13_SEL0][MFP13_SEL1][MFP13_SEL2] = 000 to select DISP. When this mode is selected, the pin is used for an LED display button function. In this mode, a normally opened switch button is connected between this pin and VSS. When the button is pressed, the pin is shorted to VSS. This pin includes an internal 18-kΩ pullup resistor to the internal LDO, which biases the pin high when the button is not pressed. The gauge monitors the pin periodically to detect when the button has been pressed, and then enables the LEDs while it is held.
unfortunately, my push-button on my film keyboard have a ~65 ohm resistance then pressed. I have ~ 1.75v on disp pin before pressing, and ~1.2v after. How can i check this 18k pull up?
If i use forceps to short pin13 to GND i can see my SOC through leds. but with my button- i can't.
I have tried to resolder IC to new one, but ,my problem still is my (
Thanks for you answer!