Part Number: BQ24780S
Hello,
this chip (BQ24780S) is present on a laptop motherboard (Asus UX305CA), but it seems not to want to charge the battery.
The computer runs on mains power, and also runs on battery power.
BUT does not charge the battery (it discharges itself until it doesn't work anymore).
I've tested the circuit continuity, and everything looks OK, plus no short circuits.
So I suspect this chip, but I don't know enough to tell if it comes from this chip or from another damaged component (resistance?)
I noted the voltages in operation with Charger + battery, and I wanted to know if the values I find are coherent or if you see something that could explain the problem...
Charger 19.5v , Battery at 11.43V
Pin 1: 19.38v
Pin 2: 19.38v
Pin 3: 19.34v
Pin 4: 19.38v
Pin 5: 1.65v
Pin 6: 0v
Pin 7 : 0v
Pin 8: 0v
Pine 9: Unknown
Pin 10: 0v
Pin 11: 3.26v
Pin 12: 3.26v
Pin 13: 0v
Pin 14: 0v
Pin 15: 1.1v
Pin 16: 11.37v
Pin 17: 11.37v
Pin 18: 11.30v
Pin 19: 11.37v
Pin 20: 0v
Pin 21: 0v
Pin 22: GND
Pine 23: 0v
Pine 24: 6.02v
Pine 25 : 11.03v
Pine 26 : 11.36v
Pine 27 : 11.36v
Pine 28: 19.14v
Thank you in advance.
Best regard
Thomas C.