Other Parts Discussed in Thread: UCC39002, UCC29002
I am using the UCC39002 current share control IC for a 2N redundant 5V at 16A application using DC-DC modules. The modules have a COMP output pin that is proportional to the output current. I am using this COMP signal as the input to the Current Sense Amp. At full load, COMP=1.35V. The gain of the CSA is three (specified minimum in the data sheet), so the CSO max = 4.05V at full load.
The issue I am having is that there is an oscillation on the ADJ line at startup. The UCC39002 specification states that the CSA is not unity gain stable, and must have a minimum gain of three. I am wondering if perhaps I am encountering the instability because the CSA is right at the lower limit of the gain spec. The oscillation looks like a relaxation oscillator and not a sinusoidal oscillation. Can anyone explain what is happening and why I'm getting an oscillation at startup? Does this oscillation look characteristic of the oscillation that might appear under unity gain? The problem only appears at startup and normal steady state operation and transient load operation all look good.
6712.5V0_SSD Current Share 2N Startup Showing Oscillation.pdf
2475.JSC Schematic Current Share.pdf
thanks,
Lance