This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3880: Sequencers Forum

Part Number: LM3880

Hello,

I have a question regarding the LM3880 PSpice model from TI.

So far, I have been able to downloaded the associated SPICE model, open and view the model, and place the LM3880 part into PSpice. I can run a PSpice simulation without errors. 

My problem is: 

The flag voltages stay at 0 Volts. I first apply Vcc = 6V followed by applying EN = 3.3V. FLAG 1,2,3 all stay low at 0V. No sequencing or any kind of operation is apparent.

How can I get this models working?

I've attached some pictures to help illustrate my issue.

Thanks

  • Hello

    I checked on my end and the model works correctly. Please note that the flags are open drian connected, which means you have to connect the other end of the resistors to a higher voltage to work.

    Regards

    Ranjani