This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Q1.
Customers use the LM3880-Q1 in cascade.
*For the circuit configuration, refer to the attached file "circuit diagram".
When EN changes like attached file,
1)LM3880-Q1 Sequence-1
2)LM3880-Q1 Sequence-2
Which is the correct Sequence?
If both are wrong, please tell me the correct Sequence.
Q2.
A cycle of 120ms is shown in Figure 15 of the LM3880-Q1 data sheet.
Is the power up/down sequence affected even if EN changed during this 120 ms cycle?
-Harukawa
yihe-san,
Thank you for your reply.
I understood about Q2 as follows.
--------------------------------------------------------------------
The EN assertion(even if it is just glitch) is not accepted at between 120ms period and there are no reset operation.
--------------------------------------------------------------------
I am satisfied with this answer.
For Q1, which of the LM3880-Q1 Sequence-1 and LM3880-Q1 Sequence-2 is the correct behavior?
I expect the answer of Q1.
-Harukawa