Part Number: BQ78350-R1
Hello,
I'm quite familiar with other older CEDV gauges, and the capacity synchronization to FCC (with RSOC=100%) at charge termination, by reaching a voltage and current threshold during charge current tapering down.
This feature is handy and always present the battery at 100% to the user.
On studying a new 7S pack based on bq78350-r2 fw 2.01 build 25, I have difficulty to reach the same sync effect and RSOC does not reach 100%.
All the battery settings are correctly set:
CEDV Gauging Configuration:
CCT=1
CSYNC=1
SC=1
Advanced Charging Algorithm - Termination Config:
Charge Term Taper Current: 40mA (meaning 400mA, because I have IPSCALE0 =1)
Charge Term Voltage = 100mV
I noted during several test that the gauge never sync when the current taper down and reach those thresholds.
On doing other tests with different settings I noted instead this:
Setting Charge Term Taper Current: 200mA (meaning 2000mA because of IPSCALE0=1), the Valid Charge Termination is met after 40s the Average Capacity is below ~116mA (meaning 1160mA)
Setting Charge Term Taper Current: 100mA (meaning 1000mA because of IPSCALE0=1), the Valid Charge Termination is met after 40s the Average Capacity is below ~60mA (meaning 600mA)
Setting Charge Term Taper Current: 80mA (meaning 800mA because of IPSCALE0=1), the Valid Charge Termination is met after 40s the Average Capacity is below ~20mA (meaning 200mA)
Please note the attached charts taken during my tests (the Remaining capacity was artificially dropped by hand before each run, in order to simplify the test).
Question:
what are exactly the conditions to met the valid charge temriation ?
The voltage threshold is ok, all cells are > 4200-100 = 4100mV
How is the current interpreted ?
Does the IPSCALE setting interfere with the calculations ?
Thanks in advance
Pietro