Part Number: BQ24172
I am using the BQ24172 to charge a 3-cell battery. I refer to the evaluation board circuit and built my PCB. The target is to charge the battery with 2A current. The input power is supplied from a 15V, 6A power adapter.
I have tested the battery by charging it with a standalone charging station at 2A current and verified it is okay.
When I switch on the power adapter, the LED (the STAT pin) light is ON without blinking. I guess it means there is no error on the circuit.
I connected an ammeter in between the battery and the PCB so that I can observer the charging current. I found that the charging current does go up to about 1.6A for a few seconds, then it drop back to 0. This iterate for a few times and then the current stopped.
The battery is originally at about 10.5V.
In the circuit I am connecting the TS equal to the evaluation board circuit by using a fixed resistor value.
I attached a table of the parameters I used on the circuit board, such as charging current, regulated voltage, and etc.
Can you give me any hints where can go wrong?
Thank you very muchCharger Prototype Calculation.xlsx