Tool/software:
HI Board designers,
I am designing my board using TPS6593 PMIC
Are there some common recommendation or observations that i should be aware?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
HI Board designers,
I am designing my board using TPS6593 PMIC
Are there some common recommendation or observations that i should be aware?
HI Board designers,
Refer below, FAQs, common queries and replies
If you are using the SK-AM62A-LP EVM with the TPS65931211-Q1 PMIC, then you can modify the hardware to change the default voltage on VDD_CORE which is supplied by the PMIC multi-phase Buck1/2/3.
The GPIO6 of the PMIC was configured to set the voltage on Buck1/2/3 with the following polarity:
During power up, the PFSM for the '1211 reads the state of GPIO6 10ms after it has enabled the 3.3V load switch. If GPIO6 is pulled up to that signal, BUCK123 will be 0.85V.
Therefore, from the PMIC perspective Pull GPIO6 HIGH to the 3.3V load switch signal
This information along with all the PMIC NVM configuration was documented in the following user's guide: https://www.ti.com/lit/pdf/slvucm3
Regards,
Sreenivasa