Other Parts Discussed in Thread: UNIFLASH, AMIC110
I have an AM335x board with McSPI flash memory. How do I flash my bootloader and application into the McSPI memory using the flashing tool provided in the PDK?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
There are multiple ways to flash the McSPI memory:
Here we give an example of using the PDK flashing tool to flash the McSPI memory on AMIC110 ICE v2. We will flash both the SBL and an application so that the application will run from the McSPI memory right after a power cycle.
1. Build an RTOS application. For this example, we chose the PDK example project: GPIO_LedBlink_iceAMIC110_armTestProject.
pdkProjectCreate.bat AM335x iceAMIC110 little gpio test arm

2. Setup the AMIC110 ICE EVM according to instructions here. Launch a debug session in CCS and connect to the board.
3. Load the flash writer to the board through CCS: C:\ti\pdk_am335x_1_0_17\packages\ti\starterware\tools\flash_writer\spi_flash_writer_AM335X.out. Then run it in CCS.
4. When the flash writer runs, CCS console will display the message below and prompts the user to choose an operation:
[CortxA8] AM335X part detected. SF: Got idcode ef 40 17 Checking if Winbond flash writer can be used.. SF: Detected W25Q64 with page size 256, total 8388608 bytes Flash page size: 256 bytes Flash sector size: 4096 bytes Starting SPIWriter. Choose Operation: Enter 1 ----> To FLASH an Image Enter 2 ----> To ERASE Flash Enter 3 ----> To EXIT
Enter 1 ----> To FLASH an Image Enter 2 ----> To ERASE Flash Enter 3 ----> To EXIT 1 Enter the File Name C:\ti\pdk_am335x_1_0_17\packages\ti\starterware\binary\bootloader\bin\am335x-evm\gcc\bootloader_boot_mcspi_a8host_release_ti.bin Enter the Offset in bytes (in HEX) 0x00000
5. Repeat step 3 to load and run the flash writer.
6. Flash the application image:
Choose Operation: Enter 1 ----> To FLASH an Image Enter 2 ----> To ERASE Flash Enter 3 ----> To EXIT 1 Enter the File Name C:\ti\pdk_am335x_1_0_17\packages\MyExampleProjects\GPIO_LedBlink_iceAMIC110_armTestProject\Debug\app Enter the Offset in bytes (in HEX) 0x20000
7. Stop the CCS debug session. Power cycle the board and LED D17 should blink within a few seconds. If the serial cable is connected, the following message will be displayed in the serial console: