This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] AM625 / AM623 / AM620-Q1 / AM62Ax / AM62D-Q1 / AM62Px / AM64x / AM243x (ALV, ALX) Design Recommendations / Custom board hardware design – VMON Power OK (POK) Module Voltages Monitored and Connection recommendations

Part Number: AM620
Other Parts Discussed in Thread: AM625, AM62P

Tool/software:

HI TI experts,

I have queries related to the POK modules for AM6x family of processors 

Supported voltage monitors 

Voltage monitors that required external voltage connection and connection recommendations 

Voltage monitor connection recommendation when not used 

  • HI Board designers, 

    Please refer below.

    Supported Voltage monitors supported:

    AM64x

    AM243x (ALV/ALX)

    AM625

    AM62A

    AM62P

    Connection recommendations when used

    VMON_VSYS

    Follow System Power Supply Monitor Design Guidelines section of processor specific data sheet. 

    VMON_1P8_SOC
    VMON_3P3_SOC

    VMON_1P8_MCU
    VMON_3P3_MCU

    Connect the relevant supply directly to the pins without filter capacitor.

    Connection recommendations when not used

    AM64x

    Rev G schematics 

    The next revision of the data sheet will have the below updates

    AM243x

    The recommendations are similar to Am64x

    AM625 Rev B data sheet recommendations

    AM62x and AM62Ax have a similar requirement. This will be updated in the next revision of the data sheet.

    AM62A

    AM62P

    Refer to the processor specific data sheet and TRM for the required information.

    FAQ reference for queries related to caps on VMON pins: 

    (+) AM2434: VMON_1P8_SOC, VMON_3P3_SOC pin, blocking cap? - Arm-based microcontrollers forum - Arm-based microcontrollers - TI E2E support forums

    VMON_1P8_SOC, VMON_3P3_SOC

    VMON_1P8_MCU, VMON_3P3_MCU

    We do not recommend a decap. This is the supply seen by the device internally. This depends on the power supply quality and customer can decide the implementation based on the supply monitor inputs routing .

    For the VMON_VSYS a filter cap is recommended at the VMON_VSYS input pin of the SOC.

    Data sheet reference 

    System Power Supply Monitor Design Guidelines

    Regards,

    Sreenivasa

  • Hi Board Designers,

    Inputs related to Power OK (POK) Modules during the power-up sequence

    (+) AM6442: Power OK (POK) Modules during the power-up sequence - Processors forum - Processors - TI E2E support forums

    The TRIM is performed by TI during the component manufacturing process in order to calibrate the POKs  ?

    I am still awaiting feedback on default states of POKs and if there is any monitoring during power up. 

    I did receive confirmation that the default state of the POK will be disabled and there is no supply monitoring during power up. 

    The POKs have to be enabled and the interrupt/ESM event configured to trigger HW action. 

    Regards,

    Sreenivasa

  • Hi Board Designers,

    Inputs related to VMON_VSYS connection:

    AM62: VMON_VSYS pin - any power sequencing requirements?

    We provide guidance on how to design an external voltage divider circuit that scales the voltage to the appropriate level and limits the current which can flow into the ESD structures. They need to follow the guidelines described in the System Power Supply Monitor Design Guidelines section of the datasheet.

    I have done some research and confirmed the VMON_VSYS pin is actually fail-safe on AM62x devices since the ESD protection circuit associated with this pin is only referenced to VSS. The resistor divider is still required to reduce the system supply voltage to an acceptable potential for the VMON_VSYS pin, but we are not concern with the minimum voltage divider impedance as way to limit injection current when the system supply ramps before the device power rails. The customer just needs to make sure their design doesn't violate the maximum recommended operating condition of 1.0V for this pin.

    The VMON_VSYS input was provided as a way for software to detect a system power failure, by allowing it to be connected to the system input power rail via an external voltage divider circuit. This could be connected to power mains if the appropriate external circuit was designed to ensure the pin never exceeds -0.3V to 2.2V under any condition, never exceeds 0V - 1.0V during normal operation, and provides the proper trigger threshold of 0.45V +/- 3%.

    Each of these voltage monitors generate an interrupt to the processor. So the internal response time is mostly a function of the customers software implementation.

    Regards,

    Sreenivasa

  • Hi Board Designers,

    Inputs related to Power OK (POK) Modules during the power-up sequence

    (+) AM6442: Power OK (POK) Modules during the power-up sequence - Processors forum - Processors - TI E2E support forums

    So by default, in the hardware tie-offs configuration, ALL POK detection is disabled. Thank you for this information.

     

    I just have one last question regarding the registers CTRLMMR_MCU_PRG_PP_0_CTRL and CTRLMMR_MCU_PRG_PP_1_CTRL

    In the TRM, it is mentioned (if pok_en_sel = 1) for the CTRLMMR_MCU_PRG_PP_1_CTRL register, but this information is not provided for CTRLMMR_MCU_PRG_PP_0_CTRL.

     

    CTRLMMR_MCU_PRG_PP_1_CTRL :

     

    CTRLMMR_MCU_PRG_PP_0_CTRL :

     

    Following your response, I assume it’s the same for the CTRLMMR_MCU_PRG_PP_0_CTRL register.

    bits [0:4] only considered when POK_EN_SEL = 1h for the CTRLMMR_MCU_PRG_PP_0_CTRL register ?

    You are correct it is the same for CTRLMMR_MCU_PRG_PP_0_CTRL.

    POK_EN_SEL needs to be set to '1' for the POK_*_EN to take effect.

    Regards,

    Sreenivasa