This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] AM2434, AM2432, AM2431 Custom board hardware design - Difference in supported peripherals, peripheral instances and IOs between ALV and ALX packages

Part Number: AM6411
Other Parts Discussed in Thread: TPS65219

Tool/software:

Hi TI Experts,

In the AM243x data sheet, i see 2 packages.

Can you summarize the difference is peripherals and IOs.

  • Hi Board Designers,

    (+) [FAQ] AM2432: ALX vs ALV - Arm-based microcontrollers forum - Arm-based microcontrollers - TI E2E support forums

    Data sheet reference for pin mapping difference:

    Pin Attributes (ALV, ALX Packages)

    AM243x Package Comparison Table (ALV vs. ALX)

    Connectivity Requirements (ALV Package)

    Connectivity Requirements (ALX Package)

    Signal Descriptions

    AM243x_ALX Package - Unsupported Interfaces and Signals

    Peripherals that are not supported by ALX package device


    DDRSS DDR4/LPDDR4 DDR Subsystem DDRSS Up to 2GB (16-bit data) with inline ECC 

    General-Purpose Memory Controller w/Error Location Module (ELM) GPMC w/ELM Up to 1GB with ECC

    SERDES0

    PCI Express Port with Integrated PHY PCIE Single Lane

    Universal Serial Bus (USB3.1 Gen1) SuperSpeed Dual-Role-Device (DRD) Port with SS PHY USB  (USB2 Only supported)
    Please refer to device Software Build sheet for details regarding USB driver support.

    MultiMedia Card/ Secure Digital Interface MMCSD0 eMMC (8-bits)

    Flash Subsystem (FSS) OSPI0 - supports QSPI-Mode Only

    VMON_3P3_MCU  and VMON_1P8_MCU VMON signals not supported 

    The EXTINTn signal is not supported by the AM243x_ALX device package.

    Reduced number of peripheral instances and IOs

    Universal Asynchronous Receiver/ Transmitter instances supported reduced from 9 (2 in MCU Domain) to 8 (1 in MCU Domain)

    General-Purpose I/O GPIO reduced from 198 Up to 148

    Multichannel Serial Peripheral Interface MCSPI reduced from 7 (2 in MCU Domain) to 4 (MAIN Domain Only)

    Enhanced Pulse-Width Modulation Module EPWM reduced from 9 to 7
    Only the PWM_A output signal is available for the EHRPWM5 instance of the ALX package type.

    Fast Serial Interface FSI_TX  reduced from 2 to 1, FSI_RX reduced from 6 to 4

    The ECAP0_IN_APWM_OUT signal is not supported by the AM243x_ALX device package.

    Inter-Integrated Circuit Interface I2C reduced from 6 (2 in MCU Domain) to 3 (MAIN Domain Only)
    Analog-to-Digital Converter ADC reduced from (12-bit resolution) to (10-bit resolution)

    TRC_DATA signal is not supported 14..23

    ADC0_VREFP and ADC0_VREFN pins not supported

    ADC0_REFP and ADC0_REFN are directly connected to VDDA_ADC0 and VSS inside the SoC. 

    The MCU_SYSCLKOUT0 and MCU_EXT_REFCLK0 signals are not supported.

    The SYNC0_OUT and CPTS0_RFT_CLK signals are not supported.

    The PRG1_IEP0_EDIO_OUTVALID signal is not supported by the AM243x_ALX device package

    Supply pins 

    VDDR_CORE PWR RAM supply

    ALV

    L10, M13

    ALX

    G5, G6, J10, J12, P14, P8, R10

     

    VDD_CORE PWR Core supply

    ALV

    J10, J12, K11, K9, L12, L8, M11, M9, N10, N8, P9

    ALX

    F11, G10, H15, H8, J9, K11, K14, L13, L9, M14, M8, N10, N9, R12, R13, R9

    VDDSHV2 PWR IO supply for IO group

    ALV

    2 R10, R8, T9

    ALX

    T11, T8, U11, U7, U8

    Note: Number of GND pins for ALX package have been reduced

    Package options:
    • ALV: 17.2mm × 17.2mm, 0.8mm pitch (441-pin) [Lidded] Flip-Chip Ball Grid Array (FCBGA)
    • ALX: 11.0mm × 11.0mm, 0.5mm pitch (293-pin) [Overmolded] Flip-Chip Chip Scale Package (FCCSP)


    EVM reference

    ALV

    https://www.ti.com/tool/TMDS243EVM

    https://www.ti.com/tool/TMDS64DC01EVM

    https://www.ti.com/tool/TMDS243DC01EVM

    https://www.ti.com/tool/RIO-DEV-PLATFORM

    ALX

    https://www.ti.com/tool/LP-AM243

    https://www.ti.com/tool/BP-AM2BLDCSERVO

    https://www.ti.com/tool/BOOSTXL-IOLINKM-8

    Regards,

    Sreenivasa

  • Hi Board Designers,

    Refer additional inputs below

    (+) TPS65219: TPS6521901 - Power management forum - Power management - TI E2E support forums

    The AM243x MCU only supports VDD_CORE=0.85V and TPS6521901 has Buck1 configured to output 0.75V so it is not a good fit. Also, the ALX package does not support VDDS_DDR so you dont need a PMIC rail configured to output 1.1V or 1.2V. 

    For AM243x in ALX package we recommend using LP87334D. https://www.ti.com/lit/pdf/slda059

    Here is a quick reference that might help to clarify but let us know if you have any questions.

    • AM64 can use either, TPS6521901 or TPS6521907. This will depend on the selected speed grade and required VDD_CORE voltage.
    • AM243 can only use PMIC variants with Buck1 configured as 0.85V because it only supports 0.85V on VDD_CORE. 

    Example connections

    (+) AM2432: MCU Domain Power - Arm-based microcontrollers forum - Arm-based microcontrollers - TI E2E support forums

    There is only a single Voltage Domain in the AM243x device which is shared between MCU and MAIN domains. This single voltage domain is then split between two PSC power domains (MCU_PSC and MAIN_PSC) which are then broken open into their multiple LPSC groupings. The separation of these two domains is to enable reset isolation, this does not translate to split voltage core voltage domains. Only MCU Domain IO and Analog supplies are isolated. The core supply is shared between MAIN and MCU domains.

    To answer your question directly, the VDD_CORE supply is shared between R5F cores (MAIN domain) and M4F core (MCU domain)

    (+) AM2431: VDDSHV5/CAP_VDDSHV_MMC1/VDDA_3P3_SDIO - Processors forum - Processors - TI E2E support forums

    1a. What is function of CAP_VDDSHV_MMC1?

    [RR] The CAP_VDDSHV_MMC1 pin is routed to the output of the integrated SDIO_LDO0 3.3V to 1.8V LDO. If this LDO is used, this pin should be used to attach a 3.3uF capacitor to provide additional low-frequency stability to this LDO voltage regulator output.

    SDIO_LDO0 is used to provide optional 3.3V or 1.8V signaling to the AM243x SDIO I/O pins depending on the status of V1P8_SIGNAL_ENA select.

    V1P8_SIGNAL_ENA is set based on the MMCSD1 host controller SD_BUS_VOLTAGE selection set during the SD Bus Power Control sequence. See 12.3.5.5.1.3 SD Bus Power Control

    Also, please see the diagram below to see this full MMC1 distribution path on the AM243x GP EVM.


    The customer will use 3.3V fixed voltage for SD Card IO(switch function of 1.8V/3.3V will not be used).

    1b. In this case, is it okay to apply 3.3V on VDDSHV5 directly?


    [RR] If the SDIO_LDO0 is unused (and VDDA_3P3_SDIO is unused), then yes, you should be powering the VDDSHV5 directly from the same SDcard digital 3.3V source.

    1c. When SDIO_LDO is not used, which VSS or 3.3uF should be connected on CAP_VDDSHV_MMC1?
    Datasheet says "The CAP_VDDSHV_MMC1 pin must always be connected via a 3.3-μF ±20% capacitor to VSS" while it also says "If SDIO_LDO is not used to power VDDSHV5, each of these balls must be connected directly to VSS.".

    [RR] In the case where the SDIO_LDIO is unused, the requirement to short VDDA_3P3_SDIO and CAP_VDDSHV_MMC1 to VSS should be followed. See AM243x datasheet, Table 6-85. Connectivity Requirements (ALV Package)

    1d. EVM schematic looks like CAP_VDDSHV_MMC1 powers VDDSHV5(Not powered from external supply). However, datasheet doesn't explain details of CAP_VDDSHV_MMC1. Datasheet says "If SDIO_LDO is not used to power VDDSHV5, each of these balls must be connected directly to VSS.", but there is no explanation about "SDIO_LDO".

    [RR] See my above reply to question 1a.

    [#2]

    2a. Is it okay to ramp up VDDA_3P3_SDIO after VDD_CORE?

    [RR] Correct. It is OK to ramp VDDA_3P3_SDIO after VDD_CORE. This will be necessary in the case of the SDcard being powered down during the voltage SD_BUS_VOLTAGE selection sequence (see my above answer to 1a)

    2b. You mentioned about VDDSHVx as below. Please make sure what about "VDDA_3P3_SDIO".

    [RR] Right. Let me clarify that. This discussion was initially considering only the VDDA_3P3_SDIO and how that powered the VDDSHV5 (MMC1) pin group. What we found was that the VDDSHV5 and VDDA_3P3_SDIO power sequence requirements currently in the datasheet can be disregarded. The datasheet sequence for these power pins should be seen as a recommended startup sequence, but not a required startup sequence. There should be no problem cycling the VDDSHV5 and VDDA_3P3_SDIO power after VDD_CORE is enabled and even after PORz de-assertion and device startup.

    We also found that the ability to sequence the VDDSHV5 before or after VDD_CORE could also be applied to all of the VDDSHVx I/O power groups.

    We still recommend that you follow this datasheet sequence normally during initial startup, but if there is a need to cycle power any of these these VDDSHVx power domains after VDD_CORE and PORz, that will not casuse problems for the device.

    Our customer would like to request for the pin attributes for AM64x in Excel format.

    Here's a link to a similar file made for AM243x device:
    /cfs-file/__key/communityserver-discussions-components-files/791/AM243x_5F00_ALV_5F00_ALX_5F00_PinAttributes.xlsx

    The purpose of the request is that he wants to make sure if those 2 families (same package ALV) can be drop in replacement by comparison of their IO information.

    Regards,

    Sreenivasa