Part Number: TDA2EXEVM
Other Parts Discussed in Thread: TDA2
Hi,
Can you please give some directions on how to share the TDA2 SPI Master (there are 4 SPI Modules that can be Master where each module has support for 4 Slaves (4 CS))? There is an API in Utils_mcspi.c that I am looking at as a reference.
Upon boots, the Radar SDK initializes 4 SPI instances using channel 0 (CS0) to set up SPI communications with the 4 attached AWRs. My questions are as follows:
1. Why is it not necessary to call Utils_mcspiOpen() during AWR Init?
2. Why static Utils_mcspiDeviceCommObj gUtils_mcspiDeviceCommObj[UTILS_MCSPI_NUM_DEVICES]; where UTILS_MCSPI_NUM_DEVICES = 8? I thought there are 4 SPI modules only.
3. In my application where I share SPI Module0 using CS1 to communicate with my slave device, I called the Utils_mcspiOpen() specifying the deviceId = 0, mcSpiDevInstNum = 0, mcSpiChannelNum = 1. This resulted in a crash during boot. Debugged into it said the FIFO has already been in use.
4. The thought in calling Utils_mcspiOpen() was because the SPI 4 instances have already been initialized during AWRs setup. I assume I need to call Open() before calling Utils_mcspiRead()/Write().
Thank you in advance,