This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5718: The maximum number of lines in a frame of am5718

Part Number: AM5718

The video input port (VIP) of am5718 uses one port A and one port B, both of which are 8bit input. If the input pixel per line is not more than 1024 points and each point is 8bit, what is the maximum number of lines in a frame?