Could you please let me know the maximum operating frequency of McBSP in SPI mode on DM6437 (SoC version 1.3)?
Pramod
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Could you please let me know the maximum operating frequency of McBSP in SPI mode on DM6437 (SoC version 1.3)?
Pramod
Pramod,
The cycle time of the McBSP is 2P and P is 8.5ns for 700Mhz device. So the max frequency of McBSP is ~58Mhz.for a DM6437-700. Please note that the hold, delay and setup times in SPI mode are higher than for the non-SPI ones and that needs to be taken into account. The slave SPI mode requires the McBSP internal 8x faster than the master clock.
Thanks,
Tai