hi all,
i am using CCS 4.2.0.10018 to develop programs for EVM6474, everything went OK (programs without BIOS)til i tried to use SYS/BIOS for a project.
Some views like outline or available packages responsiveness becomes slow.And when i create a task, it does not appear in the outline view(i have to close and reopen it multiple times until it appears), and when it appears, it has a weird name different from the one i gave it. Also for Idle module, when i use it it appears in the view, but i cannot change it's parameters, like if the interface freezes.
I am using windows xp sp3 professional version.
is there any similar bugs reported about that version? what could be the problem ?