This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSEMU560V2STM-UE: TMDSEMU560V2STM-UE failed in use

Part Number: TMDSEMU560V2STM-UE

我测试了TDI端口,发现没有波形。如果是线的问题,请问该怎么更换?

  • I tested the TDI PIN and found no waveform.  If the wire is the problem, how should I replace it?

  • Hello,

    Do you have another cable you can try? I would like to check to see if the issue is with the cable or the probe itself. If you have another probe, you can take the cable from that one and try it with the one where you see the issue.

    Thanks

    ki

  • 你好,这个 Blackhawk USB560v2 System Trace Emulator,使用CCS10调试程序出现错误,ERR230,ERR231,ERR233,ERR234,ERR235,请问这个仿真器是不是坏了?

    Hello,

    This Blackhawk USB560V2 System Trace Emulator has errors when using the CCS10 debugger, ERR230, ERR231, ERR233, ERR234 and ERR235 in turns. Is the Emulator broken?  

    Thanks

  • This Blackhawk USB560V2 System Trace Emulator has errors when using the CCS10 debugger, ERR230, ERR231, ERR233, ERR234 and ERR235 in turns. Is the Emulator broken?  

    This is a low level JTAG connectivity issue. In most cases the issue is not with the emulator but with the physical JTAG connections on the actual board. Please see:

    https://software-dl.ti.com/ccs/esd/documents/ccs_debugging_jtag_connectivity_issues.html#invalid-data-read-back

    Thanks

    ki