This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: Jumbo Packet support on AM5728 RGMII interface

Part Number: AM5728

Hi Ti,

We are using a custom board and rgmii interface between processor AM5728 and FPGA. We want to use Jumbo frames inorder to increase the speed.

But by changing mtu size from command line above 1500 B , it is throwing error saying mtu size greater than maximum.

How can we set Jumbo packet as mtu size, by enabling any support in device tree or etc.

We are using Processor SDK Linux 06_03_00_106, Linux on board.

Any guidance would be appreciated.

Regards,

Regards,

Prasanth