This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA722: vision sdk debug on ccs

Part Number: DRA722

I am try vision sdk on dra722 , after load IPU2_C0 program from CCS , I using step debug , when I step over 

    gSystem_objCommon.tsk = BspOsal_taskCreate(
                                (BspOsal_TaskFuncPtr)System_main,
                                "System main",
                                (Int32)SYSTEM_TSK_PRI,
                                gSystem_tskStack,
                                sizeof(gSystem_tskStack),
                                NULL,
                                UTILS_TSK_AFFINITY_CORE0);

processor never stop, I click suspend , PC pointer is : 

UInt32 Timer_getCount(Timer_Object *obj)
{
    UInt32 tcrr = ((TimerRegs *)Timer_module->device[obj->id].baseAddr)->tcrr;

then I click Step Into , The Warning : 

Cortex_M4_IPU2_C0: Can't Run Target CPU: (Error -1268 @ 0x1090001) Device is locked up in Hard Fault or in NMI. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.4.0.00006) 

Why?