What should be specified for the parameter (dev: part) of the usbboot command?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Keerthy-san
There has been some progress in this survey.
The purpose is to boot vxWorks via USB from the u-boot prompt.
I understand the parameters of usbboot, but I haven't booted yet.
The following is the operation log.
-----
U-Boot 2016.05-00118-gdd926c6-dirty (Nov 15 2016 - 14:42:28 +0900)
CPU : DRA752-GP ES2.0
Model: TI AM5728 IDK
Board: AM572x IDK REV 1.3B
DRAM: 2 GiB
MMC: no pinctrl for sdr104
no pinctrl for ddr50
no pinctrl for sdr50
no pinctrl for sdr25
no pinctrl for sdr12
OMAP SD/MMC: 0, OMAP SD/MMC: 1
reading uboot.env
SCSI: SATA link 0 timeout.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Found 0 device(s).
Net:
Warning: ethernet@48484000 using MAC address from ROM
eth0: ethernet@48484000
Hit any key to stop autoboot: 0
=> usb start
starting USB...
USB0: Register 2000140 NbrPorts 2
Starting the controller
USB XHCI 1.00
scanning bus 0 for devices... 2 USB Device(s) found
scanning usb for storage devices... 1 Storage Device(s) found
=> usb dev
USB device 0: Vendor: TOSHIBA Rev: PMAP Prod: TransMemory-Mx
Type: Removable Hard Disk
Capacity: 14760.0 MB = 14.4 GB (30228480 x 512)
=> usb part
Partition Map for USB device 0 -- Partition Type: DOS
Part Start Sector Num Sectors UUID Type
1 2048 30226432 db350cf0-01 0c Boot
=> ls usb 0:1
system volume information/
596376 u-boot.img
75188 mlo
65536 uboot.env
1820 uenv.txt
22752972 vxworks
65264 am572x_idk_ca15.dtb
4766132 uvxworks
found.001/
found.002/
found.000/
7 file(s), 4 dir(s)
=> usbboot ${loadaddr} 0:1
Loading from usb device 0, partition 1: Name: usbda1 Type: U-Boot
** Unknown image type
Thanks for the updates. Do you have any further questions? Or we are god to close this?
- Keerthy
Hi,
I am not sure if usbboot is identifying vxworks image. Can you try loading Linux kernel Image & try?
- Keerthy