Hello,
I am looking to interface with a Tamagawa encoder using this setup: https://www.ti.com/tool/TIDEP-0101#1
I have the example program compiled, and a working debug session by first connecting to the CortexA9 target and then loading the ".out" file in the release folder. Everything works with Tera Term as shown in the example.
Now, what if I want to do this without debugging? I would like to be able to load the program onto the board and reset it anytime much like the MSP boards or an Arduino or be able to reset it by cycling power. Is there a way to load the program onto the board and have it automatically start and run on power up? I am not experienced with these boards or processors.
Thanks,
-Tyler