Part Number: PROCESSOR-SDK-J721E
We are using the Jacinto 7 board for our application. We are using RTOS SDK and version is 07_02_00_06. We are using the new camera to get the video pipeline using single camera application. For the new camera, driver is created in imaging/sensor_drv/src directory as mentioned in the document. Document link is mentioned below:
In this doc, it is mentioned that we have to build the Imaging folder followed by sdk build.

Imaging folder is built. To build the SDK, I followed the below document. Document link is mentioned below:
In the above link, it is mentioned that we can build the sdk using the top level makefile. But there is no top level makefile in mentioned directory. When I try to set the environmental setup, it shows 'bash: setupenv.sh: No such file or directory'.
1. Is sdk build necessary one for single camera application(we built imaging and vision_apps folders successfully)?
2. If yes, how to build the RTOS SDK (version: 07_02_00_06)?
Please provide some useful links to build the RTOS SDK.