This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Cann't connect the ARM of omapL137.

HI,

When I connect the omapL137,it desplay:

Warning:

0x40000220/-2062 @ marker 13500

Warning during: Execution, OCS, 

Cannot halt the processor




Board Name: OMAPL137 XDS560 Emulator

Cpu Name: ARM9_0


Abort: Close Code Composer Studio.

Retry: Try to connect to the target again.

Cancel: Remain disconnected from the target

Diagnostic: Run diagnostic utility.

 

but DSP can be connected.

Why?