Other Parts Discussed in Thread: INA226
Hi,
I'm working on a custom design based on TDA4VM EVM. The idea is to get a minimal version of the EVM that works with the prebuilt FW/SW from the SDK.
My questions are:
1. Can I remove the ina226 current monitors without FW impact?
2. Is the io expander for bootmode pins used by SoC or only automation header? Can this io expander be removed without FW impact?
3. Also, will never boot from EEPROM. Can I remove the EEPROM without FW impact?
4. EVM has a board ID EEPROM. Is there any dependency to it? Can I remove it without FW impact?
Thanks,
David