Dear sir,

         I  am  sorry  to  bother  you  but  there  is  a  problem  that   has  been  confusing   me   for  a  long  time,  and   I   need   some   help!

        My  dsp  is  dm6437,  and  the  ndk   version  is   ndk_1_92_00_22,   I  use  the   example  "helloworld"  as  the  framework  to   create  my   own   project,    it  works;    but     when   I  test   it   for   a  long   time ,   I   found  that   it   can  only   run  for   about   one  day,   then   the  system   crashes!   Then   I   find  the  ndk  has  two  kind of   versions: the   evaluation  version   and   the   production  version.   And  it   says   that   the   evaluation    version  of  TCP/IP   Stack   restricts  uasge  of  stack  to  maximum  of   24   hours!   Is   the   version   I'm   using  now  the   evaluation  one?   How   can  I   get   the   production   version?   Do  I   need  to   rewrite  all  my   code  if   I   use  another   version  of   ndk?

       Thanks   and   please   excuse   my   poor    English  O(∩_∩)O~!

 

Regards

Jay.