This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2E: How to improve the priority of GPU access DDR?

Part Number: TDA2E

The current GPU processes images with 1280*720 resolution. If the DVR function is not enabled, the average processing time of 25 frames within one second is about 30ms. If the DVR is turned on, the average time will change to about 40ms, resulting in a frame rate of less than 25 frames. Therefore, I want to improve the priority of GPU access DDR and try to optimize it. please tell me how to modify it,Thank you