This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66AK2H12: How to use QMSS Tx Queues of the Queue Manager 2 ?

Part Number: 66AK2H12

Hi,

I would like to use QMSS Tx Queues of the Queue Manager 2. For the moment I use the QMSS Tx Queue 800 (so the Queue Manager 1), I associate this queue with the Tx channel number 0 and everything works well.

Now, I would like to use the QMSS Tx Queue 8992 (=8192+800), so which is in the Queue Manager 2. The opening of this queue goes well but I don't know which Tx channel is required for the association with the queue 8992. I know that the Queue 800 is associated with Tx channel 0, queue 801 with Tx channel 1.... and queue 831 with Tx channel 31. 

So I tried to create a Tx channel number 32 (for the queue 8992) but it does not work. 

Do you have an idea please ?

Thank you in advance and have a good day,

Félix