Part Number: SK-AM64
Hi TI.
The issue is to make the board debuggable on CCS v10.3.1.00003.
First steps:
- Power sequence: 5V, 3A: LD2, LD14, LD16 - green, passed;
- Debug probe connection (JTAG, cJTAG) from PC to emulator, 5.5MHz - passed;
- Start bootable SD card (tisdk-default-image-am64xx-evm.wic, boot config B15-B0: 00010010 01000011) image - failed;
- Actual debug session on CCS - failed.
Error connecting to the target:
(Error -2081 - (0:0:0))
Device functional clock appears to be off. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 9.3.0.00058)
Thanks,
Alexey