Part Number: PROCESSOR-SDK-J721E
Other Parts Discussed in Thread: TDA4VM
Hi.
I'm using TDA4VM EVM with Processor SDK 7.3.
I tried OSPI boot mode + eMMC(rootfs) and it seems to be working.
I worked as below.
1. OSPI
=> sf probe
=> tftp ${loadaddr} tiboot3.bin
=> sf update $loadaddr 0x0 $filesize
=> tftp ${loadaddr} tispl.bin
=> sf update $loadaddr 0x80000 $filesize
=> tftp ${loadaddr} u-boot.img
=> sf update $loadaddr 0x280000 $filesize
=> tftp ${loadaddr} sysfw.itb
=> sf update $loadaddr 0x6C0000 $filesize
=> tftp ${loadaddr} nor_spi_patterns.bin
=> sf update $loadaddr 0x3fe0000 $filesize
2. eMMC
$ chmod +x mksdboot.sh
$ umount /dev/mmcblk0*
$ udevadm control -s
$ ./mksdboot.sh --device /dev/mmcblk0
$ mkdir /mnt/emmc-rootfs
$ mount /dev/mmcblk0p2 /mnt/emmc-rootfs
$ cd /mnt/emmc-rootfs
$ tar xvf /run/media/sda/tisdk-default-image-j7-evm.tar.xz .; sync
$ cd
$ umount /mnt/*
3. boot
=> env default -f -a
=> setenv mmcdev 0
=> setenv bootpart 0:2
=> setenv dorprocboot 1
=> setenv bootcmd 'run findfdt; setenv mmcdev 0; run envboot; run check_android; if test $is_android -eq 1; then run emmc_android_boot; fi; run init_${boot}; run boot_rprocs; run get_kern_${boot}; run get_fdt_${boot}; run get_overlay_${boot}; run run_kern'
=> setenv rproc_fw_binaries '2 /lib/firmware/j7-main-r5f0_0-fw 3 /lib/firmware/j7-main-r5f0_1-fw 4 /lib/firmware/j7-main-r5f1_0-fw 6 /lib/firmware/j7-c66_0-fw 7 /lib/firmware/j7-c66_1-fw 8 /lib/firmware/j7-c71_0-fw'
=> saveenv
=> boot
4. Boot log
U-Boot SPL 2020.01-00001-g9759715674-dirty (May 25 2021 - 14:16:52 +0900)
SYSFW ABI: 3.1 (firmware rev 0x0015 '21.1.1--v2021.01a (Terrific Lla')
Trying to boot from SPI
Loading Environment from MMC... *** Warning - No MMC card found, using default environment
Starting ATF on ARM64 core...
NOTICE: BL31: v2.4(release):07.03.00.005-dirty
NOTICE: BL31: Built : 00:15:40, Apr 10 2021
U-Boot SPL 2020.01-00001-g9759715674-dirty (May 25 2021 - 14:16:19 +0900)
SYSFW ABI: 3.1 (firmware rev 0x0015 '21.1.1--v2021.01a (Terrific Lla')
Detected: J7X-BASE-CPB rev E3
Detected: J7X-VSC8514-ETH rev E2
Trying to boot from SPI
Can't get reset: -2
Ring Accelerator probed rings:286, gp-rings[96,20] sci-dev-id:235
dma-ring-reset-quirk: disabled
U-Boot 2020.01-00001-g9759715674-dirty (May 25 2021 - 14:16:19 +0900)
SoC: J721E SR1.0
Model: Texas Instruments K3 J721E SoC
Board: J721EX-PM2-SOM rev E7
DRAM: 4 GiB
not found for dev hbmc-mux
Flash: 0 Bytes
MMC: sdhci@4f80000: 0, sdhci@4fb0000: 1
Loading Environment from MMC... OK
In: serial@2800000
Out: serial@2800000
Err: serial@2800000
Detected: J7X-BASE-CPB rev E3
Detected: J7X-VSC8514-ETH rev E2
Net: K3 CPSW: nuss_ver: 0x6BA00101 cpsw_ver: 0x6BA80100 ale_ver: 0x00293904 Ports:1 mdio_freq:1000000
Warning: ethernet@46000000 using MAC address from ROM
eth0: ethernet@46000000
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc1 is current device
SD/MMC found on device 1
55 bytes read in 2 ms (26.4 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc1 ...
Core 1 is already in use. No rproc commands work
Core 2 is already in use. No rproc commands work
1513584 bytes read in 37 ms (39 MiB/s)
Load Remote Processor 6 with data@addr=0x80080000 1513584 bytes: Success!
1513584 bytes read in 37 ms (39 MiB/s)
Load Remote Processor 7 with data@addr=0x80080000 1513584 bytes: Success!
9314288 bytes read in 77 ms (115.4 MiB/s)
Load Remote Processor 8 with data@addr=0x80080000 9314288 bytes: Success!
16654344 bytes read in 351 ms (45.2 MiB/s)
89857 bytes read in 6 ms (14.3 MiB/s)
1719 bytes read in 4 ms (418.9 KiB/s)
## Flattened Device Tree blob at 82000000
Booting using the fdt blob at 0x82000000
Loading Device Tree to 00000000fdd9a000, end 00000000fdeb2fff ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x411fd080]
[ 0.000000] Linux version 5.4.40-g66cf445b76 (oe-user@oe-host) (gcc version 9.2.1 20191025 (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10))) #1 SMP PREEMPT Wed Jun 17 14:28:47 UTC 2020
[ 0.000000] Machine model: Texas Instruments K3 J721E SoC
[ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
[ 0.000000] printk: bootconsole [ns16550a0] enabled
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a0000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a0100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a1000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 31 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a1100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a3000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a3000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a3100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a3100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a4000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a4100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a5000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a5000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a5100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a5100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a6000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node c66-dma-memory@a6000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a6100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node c66-memory@a6100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a7000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node c66-dma-memory@a7000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a7100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node c66-memory@a7100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a8000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node c71-dma-memory@a8000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a8100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node c71-memory@a8100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000ac000000, size 32 MiB
[ 0.000000] OF: reserved mem: initialized node vision_apps-dma-memory@ac000000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: initialized node vision_apps_shared-memories, compatible id dma-heap-carveout
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000ce000000, size 720 MiB
[ 0.000000] OF: reserved mem: initialized node vision_apps-core-heap-memory@ce000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000fb000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@fb000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000fb100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@fb100000, compatible id shared-dma-pool
[ 0.000000] cma: Failed to reserve 512 MiB
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: Trusted OS migration not required
[ 0.000000] psci: SMC Calling Convention v1.0
[ 0.000000] percpu: Embedded 2 pages/cpu s48408 r8192 d74472 u131072
[ 0.000000] Detected PIPT I-cache on CPU0
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] CPU features: detected: EL2 vector hardening
[ 0.000000] Built 1 zonelists, mobility grouping off. Total pages: 35779
[ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=47040000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),128k(ospi.env),128k(ospi.env.backup),1m(ospi.sysfw),-@8m(ospi.rootfs);47034000.hyperbus:512k(hbmc.tiboot3),2m(hbmc.tispl),4m(hbmc.u-boot),256k(hbmc.env),1m(hbmc.sysfw),-@8m(hbmc.rootfs) root=PARTUUID=2739dd1b-02 rw rootfstype=ext4 rootwait
[ 0.000000] Dentry cache hash table entries: 524288 (order: 6, 4194304 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 262144 (order: 5, 2097152 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] software IO TLB: mapped [mem 0x9a800000-0x9e800000] (64MB)
[ 0.000000] Memory: 2584000K/2293760K available (9534K kernel code, 776K rwdata, 3840K rodata, 1728K init, 695K bss, 18446744073709261376K reserved, 0K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 960 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] GICv3: Distributor has no Range Selector support
[ 0.000000] GICv3: 16 PPIs implemented
[ 0.000000] GICv3: no VLPI support, no direct LPI support
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001900000
[ 0.000000] ITS [mem 0x01820000-0x0182ffff]
[ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[ 0.000000] ITS@0x0000000001820000: allocated 1048576 Devices @8c0800000 (flat, esz 8, psz 64K, shr 0)
[ 0.000000] ITS: using cache flushing for cmd queue
[ 0.000000] GICv3: using LPI property table @0x00000008c00c0000
[ 0.000000] GIC: using cache flushing for LPI property table
[ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x00000008c00d0000
[ 0.000000] random: get_random_bytes called from start_kernel+0x2b8/0x438 with crng_init=0
[ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[ 0.000001] sched_clock: 56 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[ 0.008359] Console: colour dummy device 80x25
[ 0.012918] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
[ 0.023588] pid_max: default: 32768 minimum: 301
[ 0.028338] LSM: Security Framework initializing
[ 0.033084] Mount-cache hash table entries: 8192 (order: 0, 65536 bytes, linear)
[ 0.040651] Mountpoint-cache hash table entries: 8192 (order: 0, 65536 bytes, linear)
[ 0.072697] ASID allocator initialised with 32768 entries
[ 0.086225] rcu: Hierarchical SRCU implementation.
[ 0.099183] Platform MSI: gic-its@1820000 domain created
[ 0.104783] PCI/MSI: /interconnect@100000/interrupt-controller@1800000/gic-its@1820000 domain created
[ 0.122218] smp: Bringing up secondary CPUs ...
[ 0.159230] Detected PIPT I-cache on CPU1
[ 0.159252] GICv3: CPU1: found redistributor 1 region 0:0x0000000001920000
[ 0.159262] GICv3: CPU1: using allocated LPI pending table @0x00000008c00e0000
[ 0.159286] CPU1: Booted secondary processor 0x0000000001 [0x411fd080]
[ 0.159334] smp: Brought up 1 node, 2 CPUs
[ 0.188677] SMP: Total of 2 processors activated.
[ 0.193481] CPU features: detected: 32-bit EL0 Support
[ 0.198734] CPU features: detected: CRC32 instructions
[ 0.210279] CPU: All CPU(s) started at EL2
[ 0.214473] alternatives: patching kernel code
[ 0.219476] devtmpfs: initialized
[ 0.227413] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.237380] futex hash table entries: 512 (order: -1, 32768 bytes, linear)
[ 0.244544] pinctrl core: initialized pinctrl subsystem
[ 0.250267] NET: Registered protocol family 16
[ 0.254987] DMA: preallocated 256 KiB pool for atomic allocations
[ 0.261452] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.276744] HugeTLB registered 16.0 GiB page size, pre-allocated 0 pages
[ 0.283596] HugeTLB registered 512 MiB page size, pre-allocated 0 pages
[ 0.290355] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.298884] cryptd: max_cpu_qlen set to 1000
[ 0.305989] vsys_3v3: supplied by evm_12v0
[ 0.310309] vsys_5v0: supplied by evm_12v0
[ 0.314944] iommu: Default domain type: Translated
[ 0.320090] SCSI subsystem initialized
[ 0.324204] mc: Linux media interface: v0.10
[ 0.328596] videodev: Linux video capture interface: v2.00
[ 0.334206] pps_core: LinuxPPS API ver. 1 registered
[ 0.339275] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.348612] PTP clock support registered
[ 0.352622] EDAC MC: Ver: 3.0.0
[ 0.356302] FPGA manager framework
[ 0.359810] Advanced Linux Sound Architecture Driver Initialized.
[ 0.366354] clocksource: Switched to clocksource arch_sys_counter
[ 0.372675] VFS: Disk quotas dquot_6.6.0
[ 0.376718] VFS: Dquot-cache hash table entries: 8192 (order 0, 65536 bytes)
[ 0.386184] Carveout Heap: Exported 512 MiB at 0x00000000ae000000
[ 0.392417] thermal_sys: Registered thermal governor 'step_wise'
[ 0.392418] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.398787] NET: Registered protocol family 2
[ 0.410170] tcp_listen_portaddr_hash hash table entries: 4096 (order: 0, 65536 bytes, linear)
[ 0.418931] TCP established hash table entries: 32768 (order: 2, 262144 bytes, linear)
[ 0.427126] TCP bind hash table entries: 32768 (order: 3, 524288 bytes, linear)
[ 0.434871] TCP: Hash tables configured (established 32768 bind 32768)
[ 0.441603] UDP hash table entries: 2048 (order: 0, 65536 bytes, linear)
[ 0.448491] UDP-Lite hash table entries: 2048 (order: 0, 65536 bytes, linear)
[ 0.455881] NET: Registered protocol family 1
[ 0.460589] RPC: Registered named UNIX socket transport module.
[ 0.466642] RPC: Registered udp transport module.
[ 0.471446] RPC: Registered tcp transport module.
[ 0.476248] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.482831] PCI: CLS 0 bytes, default 64
[ 0.487150] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[ 0.498448] Initialise system trusted keyrings
[ 0.503058] workingset: timestamp_bits=46 max_order=16 bucket_order=0
[ 0.511650] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.517921] NFS: Registering the id_resolver key type
[ 0.523096] Key type id_resolver registered
[ 0.527366] Key type id_legacy registered
[ 0.531462] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.538420] 9p: Installing v9fs 9p2000 file system support
[ 0.551174] Key type asymmetric registered
[ 0.555364] Asymmetric key parser 'x509' registered
[ 0.560372] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
[ 0.567934] io scheduler mq-deadline registered
[ 0.572561] io scheduler kyber registered
[ 0.577723] pinctrl-single 4301c000.pinmux: 94 pins, size 376
[ 0.583787] pinctrl-single 11c000.pinmux: 173 pins, size 692
[ 0.589909] pinctrl-single a40000.timesync_router: 512 pins, size 2048
[ 0.598878] k3-ringacc 2b800000.ringacc: Failed to get MSI domain
[ 0.605142] k3-ringacc 3c000000.ringacc: Failed to get MSI domain
[ 0.611470] ti-pat 31010000.pat: Found PAT Rev 1.0 with 16384 pages
[ 0.617879] debugfs: Directory '31010000.pat' with parent 'regmap' already present!
[ 0.625844] ti-pat 31011000.pat: Found PAT Rev 1.0 with 16384 pages
[ 0.632255] debugfs: Directory '31011000.pat' with parent 'regmap' already present!
[ 0.640169] ti-pat 31012000.pat: Found PAT Rev 1.0 with 16384 pages
[ 0.646581] debugfs: Directory '31012000.pat' with parent 'regmap' already present!
[ 0.654495] ti-pat 31013000.pat: Found PAT Rev 1.0 with 2048 pages
[ 0.660817] debugfs: Directory '31013000.pat' with parent 'regmap' already present!
[ 0.668729] ti-pat 31014000.pat: Found PAT Rev 1.0 with 2048 pages
[ 0.675054] debugfs: Directory '31014000.pat' with parent 'regmap' already present!
[ 0.684352] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[ 0.696139] brd: module loaded
[ 0.702048] loop: module loaded
[ 0.705578] sysfs: cannot create duplicate filename '/devices/platform/dma_buf_phys'
[ 0.713504] CPU: 0 PID: 1 Comm: swapper/0 Not tainted 5.4.40-g66cf445b76 #1
[ 0.720614] Hardware name: Texas Instruments K3 J721E SoC (DT)
[ 0.726569] Call trace:
[ 0.729065] dump_backtrace+0x0/0x140
[ 0.732800] show_stack+0x14/0x20
[ 0.736184] dump_stack+0xb4/0xf8
[ 0.739567] sysfs_warn_dup+0x5c/0x78
[ 0.743301] sysfs_create_dir_ns+0xd8/0xf0
[ 0.747480] kobject_add_internal+0x94/0x280
[ 0.751836] kobject_add+0x90/0xf8
[ 0.755306] device_add+0xdc/0x600
[ 0.758775] platform_device_add+0xfc/0x228
[ 0.763042] platform_device_register_full+0xc8/0x140
[ 0.768199] dma_buf_phys_init+0x68/0x94
[ 0.772200] do_one_initcall+0x50/0x190
[ 0.776115] kernel_init_freeable+0x194/0x22c
[ 0.780560] kernel_init+0x10/0xfc
[ 0.784028] ret_from_fork+0x10/0x18
[ 0.787681] kobject_add_internal failed for dma_buf_phys with -EEXIST, don't try to register things with the same name in the same directory.
[ 0.801724] libphy: Fixed MDIO Bus: probed
[ 0.806096] tun: Universal TUN/TAP device driver, 1.6
[ 0.811513] igbvf: Intel(R) Gigabit Virtual Function Network Driver - version 2.4.0-k
[ 0.819516] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 0.825579] sky2: driver version 1.30
[ 0.829793] VFIO - User Level meta-driver version: 0.3
[ 0.835379] i2c /dev entries driver
[ 0.839430] sdhci: Secure Digital Host Controller Interface driver
[ 0.845745] sdhci: Copyright(c) Pierre Ossman
[ 0.850392] sdhci-pltfm: SDHCI platform and OF driver helper
[ 0.856619] ledtrig-cpu: registered to indicate activity on CPUs
[ 0.863362] optee: probing for conduit method from DT.
[ 0.868634] optee: revision 3.11 (c4def2a8)
[ 0.868916] optee: initialized driver
[ 0.877690] NET: Registered protocol family 17
[ 0.882307] 9pnet: Installing 9P2000 support
[ 0.886694] Key type dns_resolver registered
[ 0.891217] registered taskstats version 1
[ 0.895404] Loading compiled-in X.509 certificates
[ 0.903845] k3-ringacc 2b800000.ringacc: Failed to get MSI domain
[ 0.910165] k3-ringacc 3c000000.ringacc: Failed to get MSI domain
[ 0.917782] ti-sci 44083000.dmsc: ABI: 3.1 (firmware rev 0x0015 '21.1.1--v2021.01a (Terrific Lla')
[ 0.937022] random: fast init done
[ 0.956443] davinci-mcasp 2ba0000.mcasp: IRQ common not found
[ 0.963669] omap_i2c 40b00000.i2c: bus 0 rev0.12 at 100 kHz
[ 0.969629] omap_i2c 40b10000.i2c: bus 1 rev0.12 at 100 kHz
[ 0.975563] omap_i2c 42120000.i2c: bus 2 rev0.12 at 100 kHz
[ 0.981559] pca953x 3-0020: 3-0020 supply vcc not found, using dummy regulator
[ 1.010867] pca953x 3-0022: 3-0022 supply vcc not found, using dummy regulator
[ 1.018944] GPIO line 481 (MCASP/TRACE_MUX_S0) hogged as output/low
[ 1.025537] GPIO line 482 (MCASP/TRACE_MUX_S1) hogged as output/high
[ 1.032374] omap_i2c 2000000.i2c: bus 3 rev0.12 at 400 kHz
[ 1.038239] omap_i2c 2020000.i2c: bus 4 rev0.12 at 100 kHz
[ 1.044136] pca953x 5-0020: 5-0020 supply vcc not found, using dummy regulator
[ 1.074714] omap_i2c 2030000.i2c: bus 5 rev0.12 at 400 kHz
[ 1.080615] omap_i2c 2040000.i2c: bus 6 rev0.12 at 100 kHz
[ 1.086450] omap_i2c 2050000.i2c: bus 7 rev0.12 at 100 kHz
[ 1.092678] ti-sci-intr interconnect@100000:interconnect@28380000:interrupt-controller2: Interrupt Router 137 domain created
[ 1.104222] ti-sci-intr interconnect@100000:interrupt-controller0: Interrupt Router 131 domain created
[ 1.113802] ti-sci-intr interconnect@100000:navss@30000000:interrupt-controller1: Interrupt Router 213 domain created
[ 1.124757] ti-sci-inta 33d00000.interrupt-controller: Interrupt Aggregator domain 209 created
[ 2.142513] j721e-pcie 2900000.pcie: host bridge /interconnect@100000/pcie@2900000 ranges:
[ 2.150988] j721e-pcie 2900000.pcie: IO 0x10001000..0x10010fff -> 0x10001000
[ 2.158466] j721e-pcie 2900000.pcie: MEM 0x10011000..0x17ffffff -> 0x10011000
[ 2.166009] j721e-pcie 2900000.pcie: PCI host bridge to bus 0000:00
[ 2.172415] pci_bus 0000:00: root bus resource [bus 00-0f]
[ 2.178021] pci_bus 0000:00: root bus resource [io 0x0000-0xffff] (bus address [0x10001000-0x10010fff])
[ 2.187711] pci_bus 0000:00: root bus resource [mem 0x10011000-0x17ffffff]
[ 2.194750] pci 0000:00:00.0: [104c:b00d] type 01 class 0x060400
[ 2.200898] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x4 may corrupt adjacent RW1C bits
[ 2.210768] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x4 may corrupt adjacent RW1C bits
[ 2.220653] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0xe8 may corrupt adjacent RW1C bits
[ 2.230612] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x3e may corrupt adjacent RW1C bits
[ 2.240577] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x92 may corrupt adjacent RW1C bits
[ 2.250539] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0xb2 may corrupt adjacent RW1C bits
[ 2.260522] pci 0000:00:00.0: supports D1
[ 2.264615] pci 0000:00:00.0: PME# supported from D0 D1 D3hot
[ 2.270486] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x84 may corrupt adjacent RW1C bits
[ 2.282098] pci 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[ 2.290283] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x3e may corrupt adjacent RW1C bits
[ 2.300242] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x3e may corrupt adjacent RW1C bits
[ 2.310200] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x3e may corrupt adjacent RW1C bits
[ 2.321643] pci_bus 0000:01: busn_res: [bus 01-0f] end is updated to 01
[ 2.328412] pci 0000:00:00.0: PCI bridge to [bus 01]
[ 2.333655] pcieport 0000:00:00.0: PME: Signaling with IRQ 33
[ 2.339717] pcieport 0000:00:00.0: AER: enabled with IRQ 33
[ 3.347431] j721e-pcie 2910000.pcie: host bridge /interconnect@100000/pcie@2910000 ranges:
[ 3.355907] j721e-pcie 2910000.pcie: IO 0x18001000..0x18010fff -> 0x18001000
[ 3.363384] j721e-pcie 2910000.pcie: MEM 0x18011000..0x1fffffff -> 0x18011000
[ 3.370916] j721e-pcie 2910000.pcie: PCI host bridge to bus 0001:00
[ 3.377321] pci_bus 0001:00: root bus resource [bus 00-0f]
[ 3.382926] pci_bus 0001:00: root bus resource [io 0x10000-0x1ffff] (bus address [0x18001000-0x18010fff])
[ 3.392794] pci_bus 0001:00: root bus resource [mem 0x18011000-0x1fffffff]
[ 3.399830] pci 0001:00:00.0: [104c:b00d] type 01 class 0x060400
[ 3.406032] pci 0001:00:00.0: supports D1
[ 3.410126] pci 0001:00:00.0: PME# supported from D0 D1 D3hot
[ 3.417569] pci 0001:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[ 3.427243] pci_bus 0001:01: busn_res: [bus 01-0f] end is updated to 01
[ 3.434009] pci 0001:00:00.0: PCI bridge to [bus 01]
[ 3.439235] pcieport 0001:00:00.0: PME: Signaling with IRQ 36
[ 3.445222] pcieport 0001:00:00.0: AER: enabled with IRQ 36
[ 4.453021] j721e-pcie 2920000.pcie: host bridge /interconnect@100000/pcie@2920000 ranges:
[ 4.461501] j721e-pcie 2920000.pcie: IO 0x4400001000..0x4400010fff -> 0x00001000
[ 4.469332] j721e-pcie 2920000.pcie: MEM 0x4400011000..0x4407ffffff -> 0x00011000
[ 4.477220] j721e-pcie 2920000.pcie: PCI host bridge to bus 0002:00
[ 4.483626] pci_bus 0002:00: root bus resource [bus 00-0f]
[ 4.489231] pci_bus 0002:00: root bus resource [io 0x20000-0x2ffff] (bus address [0x1000-0x10fff])
[ 4.498477] pci_bus 0002:00: root bus resource [mem 0x4400011000-0x4407ffffff] (bus address [0x00011000-0x07ffffff])
[ 4.509244] pci 0002:00:00.0: [104c:b00d] type 01 class 0x060400
[ 4.515447] pci 0002:00:00.0: supports D1
[ 4.519541] pci 0002:00:00.0: PME# supported from D0 D1 D3hot
[ 4.526990] pci 0002:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[ 4.536655] pci_bus 0002:01: busn_res: [bus 01-0f] end is updated to 01
[ 4.543422] pci 0002:00:00.0: PCI bridge to [bus 01]
[ 4.548645] pcieport 0002:00:00.0: PME: Signaling with IRQ 39
[ 4.554656] pcieport 0002:00:00.0: AER: enabled with IRQ 39
[ 4.561018] k3-ringacc 2b800000.ringacc: Ring Accelerator probed rings:286, gp-rings[96,20] sci-dev-id:235
[ 4.570893] k3-ringacc 2b800000.ringacc: dma-ring-reset-quirk: disabled
[ 4.577652] k3-ringacc 2b800000.ringacc: RA Proxy rev. 66346100, num_proxies:64
[ 4.586464] k3-ringacc 3c000000.ringacc: Ring Accelerator probed rings:1024, gp-rings[440,150] sci-dev-id:211
[ 4.596603] k3-ringacc 3c000000.ringacc: dma-ring-reset-quirk: disabled
[ 4.603361] k3-ringacc 3c000000.ringacc: RA Proxy rev. 66346100, num_proxies:64
[ 4.611032] omap8250 40a00000.serial: PM domain pd:149 will not be powered off
[ 4.618565] 40a00000.serial: ttyS1 at MMIO 0x40a00000 (irq = 7, base_baud = 6000000) is a 8250
[ 4.627722] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 18, base_baud = 3000000) is a 8250
[ 4.636463] printk: console [ttyS2] enabled
[ 4.636463] printk: console [ttyS2] enabled
[ 4.644900] printk: bootconsole [ns16550a0] disabled
[ 4.644900] printk: bootconsole [ns16550a0] disabled
[ 4.655269] 2810000.serial: ttyS3 at MMIO 0x2810000 (irq = 19, base_baud = 3000000) is a 8250
[ 4.664095] 2840000.serial: ttyS6 at MMIO 0x2840000 (irq = 20, base_baud = 3000000) is a 8250
[ 4.672824] arm-smmu-v3 36600000.smmu: ias 48-bit, oas 48-bit (features 0x00001faf)
[ 4.681696] arm-smmu-v3 36600000.smmu: allocated 524288 entries for cmdq
[ 4.690651] arm-smmu-v3 36600000.smmu: allocated 524288 entries for evtq
[ 4.698157] arm-smmu-v3 36600000.smmu: msi_domain absent - falling back to wired irqs
[ 4.706824] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vdd-hba-supply regulator, assuming enabled
[ 4.717332] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vcc-supply regulator, assuming enabled
[ 4.727485] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vccq-supply regulator, assuming enabled
[ 4.737723] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vccq2-supply regulator, assuming enabled
[ 4.748374] scsi host0: ufshcd
[ 4.753179] cadence-qspi 47040000.spi: unrecognized JEDEC id bytes: ff ff ff ff ff ff
[ 4.760999] cadence-qspi 47040000.spi: Cadence QSPI NOR probe failed -2
[ 4.767791] cadence-qspi: probe of 47040000.spi failed with error -2
[ 4.774140] cdns-ufshcd 4e84000.ufs: ufshcd_print_pwr_info:[RX, TX]: gear=[1, 1], lane[1, 1], pwr[SLOWAUTO_MODE, SLOWAUTO_MODE], rate = 0
[ 4.774560] cadence-qspi 47050000.spi: mt25qu512a (65536 Kbytes)
[ 4.810349] cdns-ufshcd 4e84000.ufs: ufshcd_print_pwr_info:[RX, TX]: gear=[3, 3], lane[2, 2], pwr[FAST MODE, FAST MODE], rate = 2
[ 4.822020] cdns-ufshcd 4e84000.ufs: ufshcd_find_max_sup_active_icc_level: Regulator capability was not set, actvIccLevel=0
[ 4.833303] scsi 0:0:0:49488: Well-known LUN TOSHIBA THGAF8G8T23BAILB 0300 PQ: 0 ANSI: 6
[ 4.834618] cadence-qspi 47050000.spi: Cadence QSPI NOR probe failed -517
[ 4.848870] scsi 0:0:0:49476: Well-known LUN TOSHIBA THGAF8G8T23BAILB 0300 PQ: 0 ANSI: 6
[ 4.857606] cdns-ufshcd 4e84000.ufs: ufshcd_scsi_add_wlus: BOOT WLUN not found
[ 4.886362] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[ 4.894005] libphy: 46000f00.mdio: probed
[ 4.899061] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867
[ 4.907329] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00101, cpsw version 0x6BA80100 Ports: 2
[ 4.918746] am65-cpsw-nuss 46000000.ethernet: Failed to request tx dma channel -517
[ 4.927225] am65-cpts 310d0000.cpts: CPTS ver 0x4e8a010a, freq:200000000, add_val:4 pps:0
[ 4.935740] mmc0: CQHCI version 5.10
[ 4.970104] mmc0: SDHCI controller on 4f80000.sdhci [4f80000.sdhci] using ADMA 64-bit
[ 4.978649] davinci-mcasp 2ba0000.mcasp: IRQ common not found
[ 4.989581] vdd_mmc1: supplied by vsys_3v3
[ 4.994430] omap-mailbox 31f80000.mailbox: omap mailbox rev 0x66fc7100
[ 5.001274] omap-mailbox 31f81000.mailbox: omap mailbox rev 0x66fc7100
[ 5.008103] omap-mailbox 31f82000.mailbox: omap mailbox rev 0x66fc7100
[ 5.014928] omap-mailbox 31f83000.mailbox: omap mailbox rev 0x66fc7100
[ 5.021736] omap-mailbox 31f84000.mailbox: omap mailbox rev 0x66fc7100
[ 5.030783] ti-udma 285c0000.dma-controller: Channels: 8 (tchan: 4, rchan: 4, gp-rflow: 8)
[ 5.039625] ti-udma 31150000.dma-controller: Channels: 16 (tchan: 8, rchan: 8, gp-rflow: 16)
[ 5.048814] cadence-qspi 47050000.spi: mt25qu512a (65536 Kbytes)
[ 5.094363] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[ 5.102007] libphy: 46000f00.mdio: probed
[ 5.107079] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867
[ 5.115356] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00101, cpsw version 0x6BA80100 Ports: 2
[ 5.127690] am65-cpsw-nuss 46000000.ethernet: set new flow-id-base 48
[ 5.134777] pps pps0: new PPS source ptp1
[ 5.138931] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010a, freq:500000000, add_val:1 pps:1
[ 5.147912] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 57.4
[ 5.155218] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64
[ 5.162618] mmc1: CQHCI version 5.10
[ 5.168371] mmc0: Command Queue Engine enabled
[ 5.172818] mmc0: new HS400 MMC card at address 0001
[ 5.182020] mmcblk0: mmc0:0001 S0J56X 14.8 GiB
[ 5.186722] mmcblk0boot0: mmc0:0001 S0J56X partition 1 31.5 MiB
[ 5.192735] mmcblk0boot1: mmc0:0001 S0J56X partition 2 31.5 MiB
[ 5.198655] mmc1: SDHCI controller on 4fb0000.sdhci [4fb0000.sdhci] using ADMA 64-bit
[ 5.206843] mmcblk0rpmb: mmc0:0001 S0J56X partition 3 4.00 MiB, chardev (240:0)
[ 5.214193] davinci-mcasp 2ba0000.mcasp: IRQ common not found
[ 5.226288] debugfs: Directory 'pd:242' with parent 'pm_genpd' already present!
[ 5.234223] debugfs: Directory 'pd:241' with parent 'pm_genpd' already present!
[ 5.241569] debugfs: Directory 'pd:240' with parent 'pm_genpd' already present!
[ 5.248903] debugfs: Directory 'pd:239' with parent 'pm_genpd' already present!
[ 5.256945] input: gpio-keys as /devices/platform/gpio-keys/input/input0
[ 5.263769] hctosys: unable to open rtc device (rtc0)
[ 5.275949] ALSA device list:
[ 5.278909] No soundcards found.
[ 5.282567] Waiting for root device PARTUUID=2739dd1b-02...
[ 6.668053] mmc1: new ultra high speed DDR50 SDHC card at address 59b4
[ 6.674963] mmcblk1: mmc1:59b4 NCard 15.1 GiB
[ 6.681846] mmcblk1: p1 p2
[ 6.862077] EXT4-fs (mmcblk1p2): recovery complete
[ 6.869946] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)
[ 6.878054] VFS: Mounted root (ext4 filesystem) on device 179:98.
[ 6.887348] devtmpfs: mounted
[ 6.890680] Freeing unused kernel memory: 1728K
[ 6.895222] Run /sbin/init as init process
[ 7.070847] systemd[1]: System time before build time, advancing clock.
[ 7.127047] NET: Registered protocol family 10
[ 7.131886] Segment Routing with IPv6
[ 7.149955] systemd[1]: systemd 244.3+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid)
[ 7.171713] systemd[1]: Detected architecture arm64.
Welcome to Arago 2020.05!
[ 7.219193] systemd[1]: Set hostname to <j7-evm>.
[ 7.412473] systemd[1]: /lib/systemd/system/docker.socket:6: ListenStream= references a path below legacy directory /var/run/, updating /var/run/docker.sock → /run/docker.sock; please update the unit file accordingly.
[ 7.477893] random: systemd: uninitialized urandom read (16 bytes read)
[ 7.484624] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling.
[ 7.496964] systemd[1]: (This warning is only shown for the first unit using IP firewalling.)
[ 7.506806] systemd[1]: Created slice system-getty.slice.
[ OK ] Created slice system-getty.slice.
[ 7.522431] random: systemd: uninitialized urandom read (16 bytes read)
[ 7.529626] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ 7.546410] random: systemd: uninitialized urandom read (16 bytes read)
[ 7.553555] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 7.570520] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password …ts to Console Directory Watch.
[ 7.594457] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password R…uests to Wall Directory Watch.
[ 7.618455] systemd[1]: Reached target Paths.
[ OK ] Reached target Paths.
[ 7.634408] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 7.654398] systemd[1]: Reached target Slices.
[ OK ] Reached target Slices.
[ 7.670405] systemd[1]: Reached target Swap.
[ OK ] Reached target Swap.
[ 7.693599] systemd[1]: Listening on RPCbind Server Activation Socket.
[ OK ] Listening on RPCbind Server Activation Socket.
[ 7.714433] systemd[1]: Reached target RPC Port Mapper.
[ OK ] Reached target RPC Port Mapper.
[ 7.732372] systemd[1]: Listening on Process Core Dump Socket.
[ OK ] Listening on Process Core Dump Socket.
[ 7.750529] systemd[1]: Listening on initctl Compatibility Named Pipe.
[ OK ] Listening on initctl Compatibility Named Pipe.
[ 7.778994] systemd[1]: Condition check resulted in Journal Audit Socket being skipped.
[ 7.787339] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 7.806686] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 7.822684] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 7.846581] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 7.866507] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 7.889404] systemd[1]: Mounting Huge Pages File System...
Mounting Huge Pages File System...
[ 7.909810] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 7.928541] systemd[1]: Mounting Kernel Debug File System...
Mounting Kernel Debug File System...
[ 7.949856] systemd[1]: Mounting Temporary Directory (/tmp)...
Mounting Temporary Directory (/tmp)...
[ 7.973388] systemd[1]: Starting Create list of static device nodes for the current kernel...
Starting Create list of st…odes for the current kernel...
[ 8.000611] systemd[1]: Starting Start psplash boot splash screen...
Starting Start psplash boot splash screen...
[ 8.025292] systemd[1]: Started Hardware RNG Entropy Gatherer Daemon.
[ OK ] Started Hardware RNG Entropy Gatherer Daemon.
[ 8.049545] systemd[1]: Starting RPC Bind...
Starting RPC Bind...
[ 8.066522] systemd[1]: Condition check resulted in File System Check on Root Device being skipped.
[ 8.081357] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 8.114100] systemd[1]: Starting Load Kernel Modules...
Starting Load Kernel Modules...
[ 8.133411] cryptodev: loading out-of-tree module taints kernel.
[ 8.142480] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems cryptodev: driver 1.10 loaded.
[0m...
[ 8.168799] EXT4-fs (mmcblk1p2): re-mounted. Opts: (null)
[ 8.177240] systemd[1]: Starting udev Coldplug all Devices...
Starting udev Coldplug all Devices...
[ 8.200842] systemd[1]: Started RPC Bind.
[ OK ] Started RPC Bind.
[ 8.219592] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Mounted Huge Pages File System.
[ OK ] Mounted POSIX Message Queue File System.
[ OK ] Mounted Kernel Debug File System.
[ OK ] Mounted Temporary Directory (/tmp).
[ OK ] Started Create list of sta… nodes for the current kernel.
[FAILED] Failed to start Start psplash boot splash screen.
See 'systemctl status psplash-start.service' for details.
[DEPEND] Dependency failed for Star…progress communication helper.
[ OK ] Started Load Kernel Modules.
[ OK ] Started Remount Root and Kernel File Systems.
Mounting Kernel Configuration File System...
Starting Flush Journal to Persistent Storage...
[ 8.406193] systemd-journald[227]: Received client request to flush runtime journal.
Starting Apply Kernel Variables...
Starting Create Static Device Nodes in /dev...
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Started Flush Journal to Persistent Storage.
[ OK ] Started Apply Kernel Variables.
[ OK ] Started Create Static Device Nodes in /dev.
[ OK ] Reached target Local File Systems (Pre).
Mounting /media/ram...
Mounting /var/volatile...
Starting udev Kernel Device Manager...
[ OK ] Started udev Coldplug all Devices.
[ OK ] Mounted /media/ram.
[ OK ] Mounted /var/volatile.
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Create Volatile Files and Directories...
[ OK ] Started udev Kernel Device Manager.
[ OK ] Started Create Volatile Files and Directories.
Starting Network Time Synchronization...
Starting Update UTMP about System Boot/Shutdown...
[ OK ] Started Update UTMP about System Boot/Shutdown.
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Initialization.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target System Time Set.
[ OK ] Reached target System Time Synchronized.
[ OK ] Started Daily rotation of log files.
[ OK ] Reached target Timers.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Listening on D-Bus System Message Bus Socket.
Starting Docker Socket for the API.
[ OK ] Listening on dropbear.socket.
Starting Reboot and dump vmcore via kexec...
[ OK ] Listening on Docker Socket for the API.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
[ OK ] Started Job spooling tools.
[ OK ] Started Periodic Command Scheduler.
[ OK ] Started D-Bus System Message Bus.
Starting Print notice about GPLv3 packages...
Starting IPv6 Packet Filtering Framework...
Starting IPv4 Packet Filtering Framework...
[ OK ] Started irqbalance daemon.
Starting rc.pvr.service...
Starting Login Service...
[ OK ] Started TEE Supplicant.
[ OK ] Started Reboot and dump vmcore via kexec.
[ OK ] Started IPv6 Packet Filtering Framework.
[ OK ] Started IPv4 Packet Filtering Framework.
[ OK ] Reached target Network (Pre).
Starting Network Service...
[ 9.285684] rti-wdt 2200000.rti: heartbeat 60 sec
[ 9.293777] PVR_K: 307: Read BVNC 22.104.208.318 from HW device registers
[ 9.302740] PVR_K: 307: RGX Device initialised with BVNC 22.104.208.318
[ 9.317863] [drm] Initialized pvr 1.10.5371573 20170530 for 4e20000000.gpu on minor 0
[ OK ] Started Login Service.
[ OK ] Started Network Service.
Starting Wait for Network to be Configured...
Starting Network Name Resolution...
[ 9.423968] rti-wdt 2210000.rti: heartbeat 60 sec
[ OK ] Started Network Name Resolution.
[ OK ] Reached target Network.
[ OK ] Reached target Host and Network Name Lookups.
Starting Avahi mDNS/DNS-SD Stack...
[ OK ] Started NFS status monitor for NFSv2/3 locking..
Starting Permit User Sessions...
[ OK ] Started Permit User Sessions.
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttyS2.
[ OK ] Started Serial Getty on ttyS3.
[ OK ] Reached target Login Prompts.
Starting Synchronize System and HW clocks...
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[FAILED] Failed to start Synchronize System and HW clocks.
See 'systemctl status sync-clocks.service' for details.
[ 9.755405] k3-dsp-rproc 4d80800000.dsp: assigned reserved memory node c66-dma-memory@a7000000
[ 10.119091] k3-dsp-rproc 4d80800000.dsp: configured DSP for IPC-only mode
[ 10.333111] remoteproc remoteproc0: 4d80800000.dsp is available
[ 10.514405] random: crng init done
[ 10.517808] random: 7 urandom warning(s) missed due to ratelimiting
[ OK ] Started Load/Save Random Seed.
[ 10.655468] k3-dsp-rproc 4d81800000.dsp: assigned reserved memory node c66-dma-memory@a6000000
[ 10.699712] remoteproc remoteproc0: powering up 4d80800000.dsp
[ 10.706392] remoteproc remoteproc0: Booting fw image j7-c66_0-fw, size 1513584
[ 10.718520] k3-dsp-rproc 4d80800000.dsp: DSP initialized in IPC-only mode
[ 10.730402] remoteproc0#vdev0buffer: assigned reserved memory node c66-dma-memory@a7000000
[ 10.739238] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 10.742140] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xd
[ 10.744786] remoteproc0#vdev0buffer: registered virtio0 (type 7)
[ 10.744789] remoteproc remoteproc0: remote processor 4d80800000.dsp is now up
[ 10.788347] platform 41000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1)
[ 10.838467] k3-dsp-rproc 4d81800000.dsp: configured DSP for IPC-only mode
***************************************************************
***************************************************************
NOTICE: This file system contains the following GPLv3 packages:
bash-dev
bash
bc
binutils
cifs-utils
cpio
dosfstools
elfutils
gawk
gdb
gdbserver
glmark2
gstreamer1.0-libav
gzip
less
libasm1
libbfd
libdw1
libelf1
libgdbm-compat4
libgdbm-dev
libgdbm6
libgmp10
libidn2-0
libreadline-dev
libreadline8
libunistring2
m4-dev
m4
nettle
parted
tar
which
If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
[ OK ] Started Print notice about GPLv3 packages.
[ 11.006455] remoteproc remoteproc1: 4d81800000.dsp is available
[ 11.029360] platform 41000000.r5f: configured R5F for IPC-only mode
[ 11.131168] platform 41000000.r5f: assigned reserved memory node r5f-dma-memory@a0000000
[ 11.139011] TI DP83867 46000f00.mdio:00: attached PHY driver [TI DP83867] (mii_bus:phy_addr=46000f00.mdio:00, irq=POLL)
[ 11.154405] k3-dsp-rproc 64800000.dsp: assigned reserved memory node c71-dma-memory@a8000000
[ 11.160141] am65-cpsw-nuss 46000000.ethernet eth0: Link is Down
[ 11.185658] k3-dsp-rproc 64800000.dsp: configured DSP for IPC-only mode
[ 11.194719] remoteproc remoteproc1: powering up 4d81800000.dsp
[ 11.202434] remoteproc remoteproc1: Booting fw image j7-c66_1-fw, size 1513584
[ 11.203589] remoteproc remoteproc2: 41000000.r5f is available
[ 11.214472] k3-dsp-rproc 4d81800000.dsp: DSP initialized in IPC-only mode
[ 11.226371] remoteproc1#vdev0buffer: assigned reserved memory node c66-dma-memory@a6000000
[ 11.238894] virtio_rpmsg_bus virtio1: rpmsg host is online
[ 11.241792] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0xd
[ 11.244419] remoteproc1#vdev0buffer: registered virtio1 (type 7)
[ 11.262430] remoteproc remoteproc1: remote processor 4d81800000.dsp is now up
[ 11.352983] remoteproc remoteproc3: 64800000.dsp is available
[ 11.454058] remoteproc remoteproc2: Direct firmware load for j7-mcu-r5f0_0-fw failed with error -2
[ 11.466390] remoteproc remoteproc2: powering up 41000000.r5f
[ 11.472102] remoteproc remoteproc2: Direct firmware load for j7-mcu-r5f0_0-fw failed with error -2
[ 11.489945] remoteproc remoteproc2: request_firmware failed: -2
[ 11.528010] platform 5c00000.r5f: configured R5F for remoteproc mode
[ 11.534457] remoteproc remoteproc3: powering up 64800000.dsp
[ 11.540166] remoteproc remoteproc3: Booting fw image j7-c71_0-fw, size 9314288
[ 11.552258] k3-dsp-rproc 64800000.dsp: DSP initialized in IPC-only mode
[ 11.562437] remoteproc3#vdev0buffer: assigned reserved memory node c71-dma-memory@a8000000
[ 11.574772] virtio_rpmsg_bus virtio2: rpmsg host is online
[ 11.580289] remoteproc3#vdev0buffer: registered virtio2 (type 7)
[ 11.587159] j721e-audio sound@0: pcm3168a-dac <-> 2ba0000.mcasp mapping ok
[ 11.594047] remoteproc remoteproc3: remote processor 64800000.dsp is now up
[ 11.601097] virtio_rpmsg_bus virtio2: creating channel rpmsg_chrdev addr 0xd
[ 11.630304] j721e-audio sound@0: pcm3168a-adc <-> 2ba0000.mcasp mapping ok
[ 11.657400] platform 5c00000.r5f: assigned reserved memory node r5f-dma-memory@a1000000
[ 11.771812] remoteproc remoteproc4: 5c00000.r5f is available
[ 11.886979] platform 5d00000.r5f: configured R5F for remoteproc mode
[ 11.990439] remoteproc remoteproc4: powering up 5c00000.r5f
[ 11.996053] remoteproc remoteproc4: Booting fw image j7-main-r5f0_0-fw, size 4847940
[ 12.013525] platform 5c00000.r5f: booting R5F core using boot addr = 0x0
[ 12.024451] remoteproc4#vdev0buffer: assigned reserved memory node r5f-dma-memory@a1000000
[ 12.038756] virtio_rpmsg_bus virtio3: rpmsg host is online
[ 12.044294] remoteproc4#vdev0buffer: registered virtio3 (type 7)
[ 12.054395] remoteproc remoteproc4: remote processor 5c00000.r5f is now up
[ 12.098319] platform 5d00000.r5f: assigned reserved memory node r5f-dma-memory@a3000000
[ 12.273493] remoteproc remoteproc5: 5d00000.r5f is available
[ 12.365854] remoteproc remoteproc5: Direct firmware load for j7-main-r5f0_1-fw failed with error -2
[ 12.376891] remoteproc remoteproc5: powering up 5d00000.r5f
[ 12.386187] remoteproc remoteproc5: Direct firmware load for j7-main-r5f0_1-fw failed with error -2
[ 12.399551] remoteproc remoteproc5: request_firmware failed: -2
[ 12.417243] platform 5e00000.r5f: configured R5F for remoteproc mode
[ 12.478530] platform 5e00000.r5f: assigned reserved memory node r5f-dma-memory@a4000000
[ 12.532335] remoteproc remoteproc6: 5e00000.r5f is available
[ 12.564799] remoteproc remoteproc6: Direct firmware load for j7-main-r5f1_0-fw failed with error -2
[ 12.578393] remoteproc remoteproc6: powering up 5e00000.r5f
[ 12.583992] remoteproc remoteproc6: Direct firmware load for j7-main-r5f1_0-fw failed with error -2
[ 12.598393] remoteproc remoteproc6: request_firmware failed: -2
[ 12.606325] platform 5f00000.r5f: configured R5F for remoteproc mode
[ 12.657342] platform 5f00000.r5f: assigned reserved memory node r5f-dma-memory@a5000000
[ OK ] Created slice system-weston.slice.
[ OK ] Started Weston Wayland Compositor.
[ 12.735102] remoteproc remoteproc7: 5f00000.r5f is available
[ 12.754476] remoteproc remoteproc7: Direct firmware load for j7-main-r5f1_1-fw failed with error -2
[ 12.766819] remoteproc remoteproc7: powering up 5f00000.r5f
[ 12.772446] remoteproc remoteproc7: Direct firmware load for j7-main-r5f1_1-fw failed with error -2
[ 12.788948] remoteproc remoteproc7: request_firmware failed: -2
[ OK ] Created slice User Slice of UID 0.
Starting User Runtime Directory /run/user/0...
[ OK ] Started User Runtime Directory /run/user/0.
Starting User Manager for UID 0...
[ 12.875637] remoteproc remoteproc8: b034000.pru is available
[ 12.919288] pru-rproc b034000.pru: PRU rproc node /interconnect@100000/icssg@b000000/pru@34000 probed successfully
[ OK ] Created slice system-systemd\x2dfsck.slice.
[ 13.077264] omap_rng 4e10000.trng: Random Number Generator ver. 241b34c
[ OK ] Started rc.pvr.service.
Starting weston.service...
[ OK ] Started User Manager for UID 0.
[ 13.125687] remoteproc remoteproc9: b004000.rtu is available
[ OK ] Started Session c1 of user root.
[ OK ] Started weston.service.
[ 13.159806] pru-rproc b004000.rtu: PRU rproc node /interconnect@100000/icssg@b000000/rtu@4000 probed successfully
Starting DEMO...
Starting telnetd.service...
[ OK ] Started DEMO.
[ OK ] Started telnetd.service.
[ 13.288092] pru-rproc b00a000.txpru: IRQ vring not found
[ 13.313813] pru-rproc b00a000.txpru: IRQ kick not found
[ 13.328184] remoteproc remoteproc10: b00a000.txpru is available
[ 13.374443] pru-rproc b00a000.txpru: PRU rproc node /interconnect@100000/icssg@b000000/txpru@a000 probed successfully
[ 13.443168] remoteproc remoteproc11: b038000.pru is available
Starting Save/Restore Sound Card State...
[ 13.491870] pru-rproc b038000.pru: PRU rproc node /interconnect@100000/icssg@b000000/pru@38000 probed successfully
[ OK ] Started Save/Restore Sound Card State.
[ OK ] Reached target Sound Card.
[ 13.538917] remoteproc remoteproc12: b006000.rtu is available
[ 13.559370] pru-rproc b006000.rtu: PRU rproc node /interconnect@100000/icssg@b000000/rtu@6000 probed successfully
[ OK ] Found device /dev/mmcblk1p1.
Starting File System Check on /dev/mmcblk1p1 13.590229] cdns-usb3 6000000.usb: DRD version v1 (ID: 0004024e, rev: 00000200)
0m...
[ 13.619500] pru-rproc b00c000.txpru: IRQ vring not found
[ 13.631866] pru-rproc b00c000.txpru: IRQ kick not found
[ 13.645899] remoteproc remoteproc13: b00c000.txpru is available
[ 13.662623] pru-rproc b00c000.txpru: PRU rproc node /interconnect@100000/icssg@b000000/txpru@c000 probed successfully
[ 13.675056] remoteproc remoteproc14: b134000.pru is available
[ 13.686427] pru-rproc b134000.pru: PRU rproc node /interconnect@100000/icssg@b100000/pru@34000 probed successfully
[ 13.692412] cdns-usb3 6400000.usb: DRD version v1 (ID: 0004024e, rev: 00000200)
[ 13.697452] remoteproc remoteproc15: b104000.rtu is available
[ 13.718417] pru-rproc b104000.rtu: PRU rproc node /interconnect@100000/icssg@b100000/rtu@4000 probed successfully
[ 13.737370] pru-rproc b10a000.txpru: IRQ vring not found
[ 13.754794] pru-rproc b10a000.txpru: IRQ kick not found
[ 13.766825] remoteproc remoteproc16: b10a000.txpru is available
[ 13.785832] usbcore: registered new interface driver usbfs
[ OK ] Started File System Check on /dev/m[ 13.794199] pru-rproc b10a000.txpru: PRU rproc node /interconnect@100000/icssg@b100000/txpru@a000 probed successfully
mcblk1p1.
[ 13.807961] usbcore: registered new interface driver hub
Mounting /run/media/mmcblk1p1...
[ 13.826113] usbcore: registered new device driver usb
[ 13.843319] remoteproc remoteproc17: b138000.pru is available
[ 13.854945] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller
[ 13.864083] pru-rproc b138000.pru: PRU rproc node /interconnect@100000/icssg@b100000/pru@38000 probed successfully
[ 13.866587] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 1
[ 13.889126] remoteproc remoteproc18: b106000.rtu is available
[ 13.896058] xhci-hcd xhci-hcd.2.auto: hcc params 0x200073c9 hci version 0x100 quirks 0x0000000000010010
[ 13.905198] pru-rproc b106000.rtu: PRU rproc node /interconnect@100000/icssg@b100000/rtu@6000 probed successfully
[ 13.914734] xhci-hcd xhci-hcd.2.auto: irq 511, io mem 0x06410000
[ OK ] Mounted /run/media/mmcblk1p1.
[ 13.930808] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.04
[ 13.933430] pru-rproc b10c000.txpru: IRQ vring not found
[ 13.948118] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 13.958363] usb usb1: Product: xHCI Host Controller
[ 13.966732] pru-rproc b10c000.txpru: IRQ kick not found
[ 13.970364] usb usb1: Manufacturer: Linux 5.4.40-g66cf445b76 xhci-hcd
[ 13.978559] remoteproc remoteproc19: b10c000.txpru is available
[ 13.982357] usb usb1: SerialNumber: xhci-hcd.2.auto
[ 13.993650] pru-rproc b10c000.txpru: PRU rproc node /interconnect@100000/icssg@b100000/txpru@c000 probed successfully
[ 13.994909] hub 1-0:1.0: USB hub found
[ 14.016823] hub 1-0:1.0: 1 port detected
[ 14.097785] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller
[ 14.122998] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 2
[ 14.166662] xhci-hcd xhci-hcd.2.auto: Host supports USB 3.0 SuperSpeed
[ 14.178477] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[ 14.193513] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 5.04
[ 14.210359] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 14.222363] usb usb2: Product: xHCI Host Controller
[ 14.230383] usb usb2: Manufacturer: Linux 5.4.40-g66cf445b76 xhci-hcd
[ 14.246363] usb usb2: SerialNumber: xhci-hcd.2.auto
[ 14.259046] hub 2-0:1.0: USB hub found
[ 14.265499] hub 2-0:1.0: 1 port detected
[ 14.430372] usb 1-1: new high-speed USB device number 2 using xhci-hcd
[ 14.586653] usb 1-1: New USB device found, idVendor=0451, idProduct=8142, bcdDevice= 1.00
[ 14.598019] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=1
[ 14.610021] usb 1-1: SerialNumber: 31000869DE36
[ 14.616256] hub 1-1:1.0: USB hub found
[ 14.622129] hub 1-1:1.0: 4 ports detected
[ 15.251213] am65-cpsw-nuss 46000000.ethernet eth0: Link is Up - 1Gbps/Full - flow control off
[ 15.259740] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org j7-evm ttyS2
Arago 2020.05 j7-evm ttyS2
j7-evm login:
Q1. Is there any problem with this process?
Q2. Is it okay to skip uEnv? when 1st process.
I thought OSPI would boot faster. There is little speed difference compared to MMCSD boot. (about 1-2 sec)
In TDA2x used fast boot(Early boot and late attach of remote cores) to boost boot speed.
Q3. Is there no fast boot(like TDA2x) in the Processor SDK?
Regards,
Lee.