Part Number: TDA4VM
In the SDK, the support for Deserializer DS90UB954 is not available.
Could you please provide the support files for the Deserializer DS90UB954.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VM
In the SDK, the support for Deserializer DS90UB954 is not available.
Could you please provide the support files for the Deserializer DS90UB954.
Hi Soumya,
DS90UB960 and DS90UB954 registers are all almost same, except for Port3(channel 2) and Port4(channel 3) related registers which are not there in DS90UB954 as compared to DS90UB9560 So if you look into any imaging driver of any sensor in TDA4 SDK, and if you skip say for example the below section of code, it should work also for DS90UB954
/*Select Channel 2*/
{0x4C, 0x24, 0x1},
{0x58, 0x5e, 0x1},/*Enable Back channel, set to 50Mbs*/
/*Select Channel 3*/
{0x4C, 0x38, 0x1},
{0x58, 0x5e, 0x1},/*Enable Back channel, set to 50Mbs*/
Soumya,
Which serializer are you planning to interface with ub954? Could you please provide some more details on the serdes chain?
Regards,
Brijesh