I found the NAND bus with is set to x16 by hardware. From the AM3715 Technical Reference Manual, it is set according to BOOTDEVICESIZE input pin. Which pin is the BOOTDEVICESIZE input pin? And also, which pin is the BOOTWAITSELECT input pin? I cannot find them in AM3715 datasheet and the Technical Reference Manual.
Regards,
Colman