Other Parts Discussed in Thread: OMAP3530
Hi. I designed a OMAP3530(OMAP3530DCBBA) board with a micron memory MT29C4G48MAPLCJI-6 based in BeagleBoard Rev C4. I tried to start it using the UART3. I configured SYS_BOOT pins as 1101111. I downloaded the x-loader successfully, then I downloaded the u-boot, but when the process ended, I connected to a serial console and nothing happened. I did the same thing with the beagle board C4 and worked, but my hardware didn’t. I noticed that the beagle board comes with a different micron memory part number (MT29C2G48MAKLCJI-6), this can be an issue? Is there any way to run a memory test with the x-loader in order to check whether the pop memory was successfully soldered and functional?