Other Parts Discussed in Thread: OMAP3530
Hello, I'm currently evaluating which CPU to use for a new design.
I've been looking at the OMAP3530 as a possible candidate and I have some questions about issues that are not clear in the datasheet. My design requires industrial temperature range. Acorrding to the datasheet OPP5&OPP6 are not supported for industrial temp. range but then there is the following comment:
"*If an extended temperature device is operated such that Tj never exceeds 90C (-40°C £Tj £ 90°C) then the OPP POH limits for commercial devices indicated above apply."
This leaves me somewhat confused. So what I want to know is this - if I use the OMAP3530DCUSA and make sure that my design does not go above Tj>90C can I use OPP5? I also see the 720MHz Cortex is never offered for devices with extended temp. range. Is this due to the fact that OPP6 isn't supported for temp. range above 90C? If I make sure my design doesn't go above Tj above 90C does TI offer any product that can work at 720MHz?
Looking forward to hear from you,
Elad